AD73322: FAQ

  • Created
  • Updated
Was this helpful?
  • AD73322/AD73322L compatibility

    Question Can I use the AD73322L as a replacement for the AD73322 and is it pin and software compatible? Answer The AD73322L is a cost reduced version of the AD73322 and is fabricated on a 0.35um process…
  • AD73322: CD measurability

    Question I want to make measurements at the tachometer output from dc-motors. This signal is a dc-voltage with ac-parts (if the motor accelerate or stop). The bandwith is therefore dc-max 2kHz. Can…
  • AD73322: Vref transfer function

    Question Are the Vref directly connected to internal non inverting input of the op, or this is an principle schematic and the output op signal are only biased with Vref. In other word is the transfer…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.