Question Would the AD7280 work with 3 cells if a cell has:
Nominal Voltage: 3.7V
Cut-Off Voltage: 2.7V
Continuos Current: 150.0A
3*2.7V=8.1V – which is 100mV above the 8V min – and this in general…
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question