AD

  • Created
Was this helpful?
  • AD1862

    Question It seems the AD1862 datasheet doesn't contain the output voltage compliance value. What is its value? Answer It's not given in the datasheet because the current output should drive the virtual…
  • AD1862: FAQ

    AD1862: FAQ
  • AD53500: FAQ

    AD53500: FAQ
  • AD53500: Thermal questions

    Question Thermal questions We use in one of our product the AD53500 driver, and we notice that these components produce a lot of heat in static mode that is to say with a fixed voltage on the input…
  • AD5934 questions - measuring inductive reactance

    Question AD9834: I have been going through the datasheet and this seems perfect device for my needs, however i did not see explicit mentioning of measuring inductive reactance. I am interested in setting…
  • AD7124: FAQ

    AD7124: FAQ
  • AD8380: FAQ

    AD8380: FAQ
  • AD8380: General conditions for various PINS

    Question I continuous to test the AD8380 and found one problem. I found the positive cycle and negative cycle are not symmetric to VMID when the input code is lower but for large input code seems better…
  • AD846 - open loop transimpedance can be reduced?

    Question I have a question concerning the AD846, regarding the simplified schematic of the AD846 from datasheet. The amplifier has an open loop transimpedance of 200MOhm. I would like to decrease this…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.