Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    A 16T/16R X-Band Direct Sampling Phased Array Subsystem using Apollo MxFE

    Join our webinar on the Quad Apollo Platform, a cutting-edge solution for accelerating high-performance digital beamforming. Discover the ADXBAND16EBZ...
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    ​​Where Errors Lurk in the GMSL Signal Chain​

    Whether you're debugging a stubborn camera link or designing a robust system from scratch, knowing where errors hide is half the battle. GMSL provides...

     

    Achieving Power Over Data with RS-485 Transceivers

    By Bryson Barney What if a single wire could carry both energy and information seamlessly—without either getting in the way? The future of connectivity...

    Latest Blogs

    • ​​Functional Safety: A Driver of “Shift Left”​
    • The 5 Advantages of Hardware Fault Tolerance
    • The Power Problem Inside Every AI Breakthrough: Part 1 of 3
    • Simplifying Stability with EVAL-KW4503Z: Part 1 of 3
    • Energy Transfer Considerations in Isolated SMPS: Part 2 of 4
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
Optical Sensing Library
Optical Sensing Library
Documents Is the MAXM86161 module suitable for monitoring infant heartbeats, heart rate variability, and SpO2?
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • +MAX86141AENP+T: FAQ
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • -MAXM86161EVSYS#: FAQ
    • Can I flash the MAXM86161EVSYS with the original .msbl file v30.2.3 that is compatible with the GUI again?
    • Can I measure HRV and SPO2 by using MAXM86161 EVSYS?
    • For MAXM86161EVSYS, how to connect the OSBFLEX PCB to MAXM86161ADPTR board?
    • Is the MAXM86161 module suitable for monitoring infant heartbeats, heart rate variability, and SpO2?
    • What is the use of MAXM86161ADPTR board in MAXM86161EVSYS?
    • When I try to connect to the MAXM86161EVSYS it asks for a firmware update, is this normal?
    • Where can I find the bare metal C library for the MAXM86161?
    • ​​​​​​​What is the function of 3-AXIS Sensor KX122 in MAXM86161EVSYS? Can I use other kind of 3-AXIS sensor and connect it to the I2C interface of MCU, rather than connecting it to MAX32664?

Is the MAXM86161 module suitable for monitoring infant heartbeats, heart rate variability, and SpO2?

The MAXM86161 module and its algorithm have not been validated for use in infants, necessitating self-validation to ensure suitability for measuring infant heartbeats and SpO2. For infants, the sensor should primarily be placed on the foot to measure heart rate and SpO2 using Red and IR LEDs. Medical certification is typically done at the system level, meaning the ability to qualify for certification by medical bodies will depend on the overall device design and the components used.

Tags: MAXM86161 Optical Sensing Technology Optical Modules