Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

Optical Sensing Library
Optical Sensing Library
Documents Is there a known issue with LED current drift?
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • -MAX86141AENP+T: FAQ
    • Are there any issues with the MAX86141 LED driver?
    • For MAX86141,Which PD and LED does maxim recommend?
    • For the HW design of MAX86141, can the Gsensor be connected to the main MCU instead of the sensor Hub MAX32664?
    • How can I use just one photodiode in the MAX86141?
    • How PI parameter works for HR and SpO2 algorithms?
    • Is there a known issue with LED current drift?
    • Maxim bio sensor algorithm takes very long time to report HR/SpO2 data.
    • Should I align the optical center of the LEDs for the wrist based SPO2 monitoring wearable design?
    • What does FDM/CDM fliter mean in MAX86141?
    • What is the requirement for algorithim to output stable SpO2 output?
    • What is the total input power requirement for the MAX86141?
    • What SPI mode does the MAX86141 use for communication?
    • Why can't the MAX86141 driver automatically adjust LED brightness after successfully porting the driver code?
    • Why we need to do calibration for SpO2 algorithm? Is it workable without calibration?
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

Is there a known issue with LED current drift?

LED thermal drift is normally expected within the first few minutes of operation due to the heating of the LED package, especially when driven with high current or long integration times (TINT). As the LED temperature increases, its luminous intensity decreases over time, leading to a reduction in photodetector current readings. Consequently, even with a constant LED current driven by the AFE, the PPG reading (ADC counts) diminishes over time.

To mitigate this, it is recommended to collect data for about 1 minute (or longer) and wait for the LED temperature to stabilize. Applying a first-order polynomial fit to the last 10 seconds of data can further reduce the effects of LED temperature drift when calculating the signal-to-noise ratio (SNR) of the application.

Tags: KB-18292 MAX86141 ppg afe Optical Sensing Library LED Current Drift Show More
  • Share
  • History
  • Cancel
 
Related Content
  • LED
    LED
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • RE: ADPD103 Drives a LED ( 5V~7V@20mA )
    ADIApproved
    Hello, The maximum voltage that can be applied at the LEDX pin is 3.6V. If the voltage of the pin is pulled above that voltage it could result in damage to the device. There are two things to watch for...
  • RE: ADPD1080 work from CR3032 battery
    Magnetron
    Assuming the LED duty cycle is low , i.e. the LED on time is very much smaller that the LED off time , then a similar technique to that used in Infra Red Remote control units for a TV can be used . The...
 
Related Content
  • LED
    LED
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • RE: ADPD103 Drives a LED ( 5V~7V@20mA )
    ADIApproved
    Hello, The maximum voltage that can be applied at the LEDX pin is 3.6V. If the voltage of the pin is pulled above that voltage it could result in damage to the device. There are two things to watch for...
  • RE: ADPD1080 work from CR3032 battery
    Magnetron
    Assuming the LED duty cycle is low , i.e. the LED on time is very much smaller that the LED off time , then a similar technique to that used in Infra Red Remote control units for a TV can be used . The...