Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Calibration Implementation Techniques for Multichannel Phased Array Subsystems

    Learn about phase-calibration techniques used for characterizing a 16 transmit and 16 receive X-band phased array subsystem based on a mixed-signal front...

Optical Sensing Library
Optical Sensing Library
Documents Error Message "Unable to load DLL 'PSnrACDC.dll': The specified module could not be found." while launching software
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • -MAX86140EVSYS#: FAQ
    • After installing the software by following the procedure in the evkit datasheet, I can see the COM port . However, there is no response after pressing "connect," and the MAX86140EVSYS cannot be connected. Why is that?
    • Error Message "Unable to load DLL 'PSnrACDC.dll': The specified module could not be found." while launching software
    • How does the timestamp is formatted and generated on the MAXSENSORBLE_EVKIT board for the some of the PPG sensor's Evaluation Kits?
    • How to upgrade MAXSensorBLE F/W using the MRD100HDK
    • In the MAX86140EVSYS, do you use a standard heart rate service defined by the SIG or it is a custom service with custom characteristics? and which Bluetooth version is implemented?
    • What battery is recommended for use with the MAX86140EVSYS?
    • What Bluetooth dongle is compatible with the MAX86140EVSYS?
    • Which are the available dongles required for the MAX86140EVSYS?
    • Why I can not run the MAX86140EVSYS on my Windows 7 Operating system?
    • Why is MAX86140EVSYS GUI PPG Plot Data Information not showing PSNR, PSNR Avg, AC, DC?
  • MAX86141AENP+: FAQ
  • +MAX86141AENP+T: FAQ
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

Error Message "Unable to load DLL 'PSnrACDC.dll': The specified module could not be found." while launching software

It has been identified that some of the bio sensor evaluation kits and MAXREFDES solutions software GUIs show the following error when the application is starting:
 
 
 

This has been linked to the 32-bit version of the Visual C++ Redistribute Packages for Visual Studio 2013, which needs to be installed for the Software GUI to work.

Download and install the x86 (32-bit) version of the Visual C++ Redistributable Packages for Visual Studio 2013.

https://www.microsoft.com/en-us/download/details.aspx?id=40784

Tags: MAX86171EVKIT evaluation software error message MAX86140EVSYS# PSnrACDC.dll evaluation kit Unable to Load DLL unable to use GUI KA-16881 dll ppg sensor software PSNRADC.DLL reference design maxrefdes104 evkit MAX86140EVSYS Show More
  • Share
  • History
  • Cancel
 
Related Content
  • Visual Analog Canvas: Unable to load DLL 'libiio.dll':The specified module could not be found
    Xifeng
    Visual Analog Canvas Visual Analog Canvas: Unable to load DLL 'libiio.dll':The specified module could not be found 1. libiio.dll is in the C:\Windows\System32 folder. 2. Found the sample in a old...
  • RE: Visual Analog doesn't find libiio.dll, but libiio is installed in the computer.
    mhennerich
    Can you try to also install the Visual C++ Redistributable Packages for Visual Studio 2013 ? -Michael
  • RE: Visual Analog doesn't find libiio.dll, but libiio is installed in the computer.
    Xifeng
    I tried all these steps. Still getting the same error 'Unable to load DLL 'libiio.dll':The specified module could not be found" Can you help me out? I use MS Windows
 
Related Content
  • Visual Analog Canvas: Unable to load DLL 'libiio.dll':The specified module could not be found
    Xifeng
    Visual Analog Canvas Visual Analog Canvas: Unable to load DLL 'libiio.dll':The specified module could not be found 1. libiio.dll is in the C:\Windows\System32 folder. 2. Found the sample in a old...
  • RE: Visual Analog doesn't find libiio.dll, but libiio is installed in the computer.
    mhennerich
    Can you try to also install the Visual C++ Redistributable Packages for Visual Studio 2013 ? -Michael
  • RE: Visual Analog doesn't find libiio.dll, but libiio is installed in the computer.
    Xifeng
    I tried all these steps. Still getting the same error 'Unable to load DLL 'libiio.dll':The specified module could not be found" Can you help me out? I use MS Windows