Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
  • Forums

    Popular Forums

    • LTspice
    • RF and Microwave
    • Video
    • Power Management
    • Precision ADCs
    • FPGA Reference Designs
    • Linux Software Drivers

    Product Forums

    • Amplifiers
    • Microcontrollers
    • Clock and Timing
    • Data Converters
    • Direct Digital Synthesis (DDS)
    • Energy Monitoring and Metering
    • Interface and Isolation
    • MEMS Inertial Sensors
    • Power Management
    • Processors and DSP
    • Switches/Multiplexers
    • Temperature Sensors
    • Voltage References
    View All

    Application Forums

    • A2B
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
    • Design Tools and Calculators
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
    The Burning Question: How can ADI Solutions Ensure Rechargeable Device Batteries are Genuine?

    On the global stage, products and equipment using rechargeable batteries continue to proliferate exponentially, expecting to reach a staggering $170B market...
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
    • Maximize Your Power Regulator: Key Considerations for Thermal Performance
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quizzes AQQ294 about a digital phase splitter design

      1. Quote of the month: "I've learned that people will forget what you said, people will forget what you did, but people will never forget how you made...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Let's Take a Field-Bus Trip Your field-bus engines...
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
    Ethernet-APL’s Impact on Functional, Intrinsic, and Cyber Safety

    Power limitations have always plagued process sensors, whether because of intrinsic safety requirements (safety achieved through power limitation) or because...

     

    Balancing Enhanced Radar Resolution with FPGA-Based Pulse Compression

    Radar and sonar systems must balance range resolution with the energy required for reliable detection. Pulse compression resolves this by sending a long...

    Latest Blogs

    • ​​ISO 26262 Essentials: Ensuring Confidence in Your Software Tools ​
    • Step-by-Step: Implementing a Complete DSP Chain for Signal Analysis
    • Galvanic Isolation in SMPS: Ensuring Safety and Protection: Part 1 of 4
    • Mature, Not Old! The Longevity of 4 – 20 mA
    • Turning up the Noise: .NOISE Simulations in LTspice: Part 1 of 3
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
Optical Sensing Library
Optical Sensing Library
Documents In PPG monitor, is Yellow LED used and what is the advantage?
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • -MAX30101ACCEVKIT#: FAQ
    • After unzipping the file "MAX30101ACCEVKIT_PCBA.ZIP" I could not find the Gerber files. Can you please advise?
    • Are there recommendations for power sequencing, isolation, and temperature management for the MAX30101/2?
    • Can 3.3V logic be used for the I2C pins of the MAX30101 even though VDD is 1.8V?
    • Can Maxim provide the MAX30101 LED location and package details?
    • Can the IR sensor of the MAX30101 be used to measure body temperature?
    • For MAX30101, is it necessary to add extra light barrier between chip glass and phone glass?
    • How can a customer package a MAX30101 to be used underwater?
    • How can PPG signal quality be improved when measured on the wrist?
    • How do I configure MAX30101 in Multi-LED Mode?
    • How do I convert the "Time" output in the log output by the MAX30101ACCEVKIT into seconds?
    • How do I read the FIFO of MAX30101?
    • How do I set the sample rate for SpO2 measurements in multi-LED mode for the MAX30101?
    • How do I set up interrupt for MAX30101/MAX30102 for reading data?
    • How to select the green LED only on the MAX30101
    • If I enable sample averaging in MAX30101/MAX30102 and keep the sampling rate setting to be the same, does the effective sampling rate go down?
    • In PPG monitor, is Yellow LED used and what is the advantage?
    • Is it possible to directly use the daughter board (MAX30101DBEVKIT) with an alternate microcontroller for evaluation, without connecting to the motherboard (USBOSMB)?
    • MAX30101 UV tolerant?
    • What are the factors that makes impact on the time delay between AFE conversion start time and  PPG Data Ready ?
    • What Cover Material Can I Use for the MAX30101, MAX30102, or MAX30105?
    • What is the sampling rate assumed in the PBA algorithm provided for the MAX301xx optical sensors?
    • Which Maxim Pulse Oximeters integrate Red/IR LEDs?
    • Why do the green and red LEDs on the mother board keep flashing, when using the MAX30101ACCEVKIT?
    • Why is the MAX30101 green LED not lighting?
    • Why is the PPG signal saturated when using the MAX30101, MAX30102, or MAX30105?
    • Why is the time taken for an initial result of HR and SpO2 different ?
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • +MAX86141AENP+T: FAQ
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

In PPG monitor, is Yellow LED used and what is the advantage?

Green/Yellow optical sensor array can provide superior measurement with all skin tones. Better than monitors and watches that employ only green sensors.
Tags: KA-16480 ppg optical sensing Yellow LED max30101
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
©2025 Analog Devices, Inc. All Rights Reserved
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
©2025 Analog Devices, Inc. All Rights Reserved