Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Other Products Library
    • Precision Technology Signal Chains Library
    • Software Modules and SDKs Library
    • Supervisory Circuits Library
    • Wireless Sensor Networks Library

    Latest Webinars

    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      KCC's Quizzes AQQ297 about taking the right dose of medication

      1. First, the quote of the month: " All my life I though air is free until I bought a bag of chips " - unknown 2. New quiz AQQ297 about taking the right...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Charting Calm Seas: Tips for Robust RS-485 Data Transmission

    by Bryson Barney As our world becomes ever more dependent on flawless digital communication, engineers need to find new ways of charting calm seas when...

     

    Unpacking IEC 61508: Low Complexity versus Type A Made Simple

    IEC 61508 appears to include two very similar concepts. Type A and simple, which is referred to as “low complexity”. Anything that isn’t low complexity...

    Latest Blogs

    • Taming the AI Power Storm: Part 2 of 3
    • TIA Me Up, But Keep It Stable: Part 2 of 3
    • Celebrating Innovation: Top 3 EngineerZone Spotlight Blogs from 2025
    • Transforming Power: Transfer Techniques in SMPS: Part 3 of 4
    • Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3
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
Optical Sensing Library
Optical Sensing Library
Documents Why is MAX86140EVSYS GUI PPG Plot Data Information not showing PSNR, PSNR Avg, AC, DC?
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • -MAX86140EVSYS#: FAQ
    • After installing the software by following the procedure in the evkit datasheet, I can see the COM port . However, there is no response after pressing "connect," and the MAX86140EVSYS cannot be connected. Why is that?
    • Error Message "Unable to load DLL 'PSnrACDC.dll': The specified module could not be found." while launching software
    • How does the timestamp is formatted and generated on the MAXSENSORBLE_EVKIT board for the some of the PPG sensor's Evaluation Kits?
    • How to upgrade MAXSensorBLE F/W using the MRD100HDK
    • In the MAX86140EVSYS, do you use a standard heart rate service defined by the SIG or it is a custom service with custom characteristics? and which Bluetooth version is implemented?
    • What battery is recommended for use with the MAX86140EVSYS?
    • What Bluetooth dongle is compatible with the MAX86140EVSYS?
    • Which are the available dongles required for the MAX86140EVSYS?
    • Why I can not run the MAX86140EVSYS on my Windows 7 Operating system?
    • Why is MAX86140EVSYS GUI PPG Plot Data Information not showing PSNR, PSNR Avg, AC, DC?
  • MAX86141AENP+: FAQ
  • +MAX86141AENP+T: FAQ
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

Why is MAX86140EVSYS GUI PPG Plot Data Information not showing PSNR, PSNR Avg, AC, DC?

Revision Creation Date Revision Author
Current Revision 10 Feb 2026 2:34 PM MSDAPI
Revision #3 10 Feb 2026 2:34 PM MSDAPI
Revision #2 19 Dec 2023 7:04 PM MSDAPI
Revision #1 31 Jan 2022 11:04 PM MSDAPI
  • Compare Versions View current version