Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

Optical Sensing Library
Optical Sensing Library
Documents When I use the MAX30102EVKIT software, it crashes due to a pba.dll error. How do I fix this?
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • -MAX30102ACCEVKIT#: FAQ
    • Is there Software for the MAX30102ACCEVKIT that runs on Mac OS?
    • What is the difference between the MAX30101ACCEVKIT# and MAX30102ACCEVKIT#?
    • What Prevents "USB HID Report Timeout" Errors with the MAX30102ACCEVKIT?
    • When I use the MAX30102EVKIT software, it crashes due to a pba.dll error. How do I fix this?
    • Why is the MAX30101_xxxxx.csv missing HR and SpO2 samples when using the eval kit GUI?
    • Why is the message "HR/SPO2 only valid for Fs=100Sps" displayed in the MAX30102ACCEVKIT GUI?
    • Why is the VLED+ voltage on the MAX30102ACCEVKIT at 4.4V?
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • +MAX86141AENP+T: FAQ
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

When I use the MAX30102EVKIT software, it crashes due to a pba.dll error. How do I fix this?

Please look at the installation directory of MAX30102EVKIT and see if PBA.dll is stored in the directory. If it missing, please uninstall and reinstall the software package.

Tags: MAX30102ACCEVKIT# software PBA.dll dll MAX30102 KA-16062 Show More
  • Share
  • History
  • Cancel
 
Related Content
  • The MAX30102ACCEVKIT GUI keeps crashing while trying to find the pba.dll file, but it is installed correctly, what could be the issue?
    MSDAPI
    Please i nstall the relevant Microsoft Visual C++ redistribute package for your OS at the below link. https://www.microsoft.com/en-us/download/details.aspx?id=40784
  • RE: SDP-S DLL and/or LabVIEW Examples
    mattzimm85
    I installed the AD5535 Eval Software and I believe the DLL for the SDP-S was installed to the same folder as the evaluation software executable. For me it was C:\Program Files (x86)\AD5535B The DLL name...
  • RE: 64 bit adiclockeval.dll for AD9910 evaluation board
    ADIApproved
    Hi Yu, I personally do not have the copy of a 64 bit version of the dll. However, I'd like to suggest to use CyUSB.dll which is a more generic version of this adiclockeval.dll. We do not expose the documentation...
 
Related Content
  • The MAX30102ACCEVKIT GUI keeps crashing while trying to find the pba.dll file, but it is installed correctly, what could be the issue?
    MSDAPI
    Please i nstall the relevant Microsoft Visual C++ redistribute package for your OS at the below link. https://www.microsoft.com/en-us/download/details.aspx?id=40784
  • RE: SDP-S DLL and/or LabVIEW Examples
    mattzimm85
    I installed the AD5535 Eval Software and I believe the DLL for the SDP-S was installed to the same folder as the evaluation software executable. For me it was C:\Program Files (x86)\AD5535B The DLL name...
  • RE: 64 bit adiclockeval.dll for AD9910 evaluation board
    ADIApproved
    Hi Yu, I personally do not have the copy of a 64 bit version of the dll. However, I'd like to suggest to use CyUSB.dll which is a more generic version of this adiclockeval.dll. We do not expose the documentation...