Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    • LiDAR Solutions
    • Motor Control Hardware Platforms
    • Speech Processing Solutions
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
    Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      KCC's Quizzes AQQ301 - Counting Bicycles and Tricycles

      1. Quote of the month: " People who didn't need people needed people around to know that they were the kind of people who didn't need people" - Terry Pratchett...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 2: Achieving Phase Repeatability

    This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...

Optical Sensing Library
Optical Sensing Library
Documents Do activity classifier, step counter, and energy expenditure features in MAXM86161 algorithm work for in-ear applications?
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • +MAX86141AENP+T: FAQ
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • -MAXM86161EFD+: FAQ
    • Do activity classifier, step counter, and energy expenditure features in MAXM86161 algorithm work for in-ear applications?
    • How do you monitor sudden DC shift in the ADC value on the MAXM86161?
    • Is it necessary to use 12 layers layout for MAXM86161 design?
    • Is there any filling inside the module of the MAXM86161?
    • What are the main differences between the MAXM86161 and the MAX86160?
    • What is the purpose of the LDO present on the MAXM86161?
    • What is the purpose of the sub-DAC tag on the MAXM86161?
    • When I use MAXM86161 to measure HR and SpO2, Where is the best location for the sensor module?
    • When measuring HR and SpO2 by MAXM86161, how long it will take to obtain reliable measurement results? MAXM86161 is an in-ear product, but how is the accuracy of the result when compared with the arm?
    • Which version of the MAX32664 is compatible with the MAXM86161?
  • +MAXM86161EVSYS#: FAQ

Do activity classifier, step counter, and energy expenditure features in MAXM86161 algorithm work for in-ear applications?

The algorithms for the Activity Classifier, Step-Counter, and Energy Expenditure were only developed for the wrist-based applications. In the firmware version v32.9.22 of the MAXM86161, the output values of these features are still reported in the extended algorithm output during in-ear measurements, but they might be inaccurate and should not be used.

Tags: MAXM86161 In-ear Energy Expenditure MAXM86161EFD+ Optical Sensing Technology Sensors and MEMS Step Counter KA-16036 Activity Classifier Show More