Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Fast-Track Certification: Leveraging IC Safety App Notes for Functional Safety Designs
    View All Webinars
  • Community Hub

    Challenge Yourself!

      World Engineering Day Quiz!

      By Kuo-Chang A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

Optical Sensing Library
Optical Sensing Library
Documents How does the timestamp is formatted and generated on the MAXSENSORBLE_EVKIT board for the some of the PPG sensor's Evaluation Kits?
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • -MAX86140EVSYS#: FAQ
    • After installing the software by following the procedure in the evkit datasheet, I can see the COM port . However, there is no response after pressing "connect," and the MAX86140EVSYS cannot be connected. Why is that?
    • Error Message "Unable to load DLL 'PSnrACDC.dll': The specified module could not be found." while launching software
    • How does the timestamp is formatted and generated on the MAXSENSORBLE_EVKIT board for the some of the PPG sensor's Evaluation Kits?
    • How to upgrade MAXSensorBLE F/W using the MRD100HDK
    • In the MAX86140EVSYS, do you use a standard heart rate service defined by the SIG or it is a custom service with custom characteristics? and which Bluetooth version is implemented?
    • What battery is recommended for use with the MAX86140EVSYS?
    • What Bluetooth dongle is compatible with the MAX86140EVSYS?
    • Which are the available dongles required for the MAX86140EVSYS?
    • Why I can not run the MAX86140EVSYS on my Windows 7 Operating system?
    • Why is MAX86140EVSYS GUI PPG Plot Data Information not showing PSNR, PSNR Avg, AC, DC?
  • MAX86141AENP+: FAQ
  • +MAX86141AENP+T: FAQ
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

How does the timestamp is formatted and generated on the MAXSENSORBLE_EVKIT board for the some of the PPG sensor's Evaluation Kits?

For all the evaluation kits (MAXM86161EVKIT/SYS, MAXM86146EVKIT/SYS, MAX86176EVSYS, MAX86171EVSYS, MAX86140/1EVSYS)
that contain the MAXSENSORBLE_EVKIT board, the timestamp format and how timestamps are generated is explained in the following summary:

Format
The timestamps are in milliseconds (ms) from the epoch (converter).

Generation
FW logic:

  1. SW sends wall clock time
  2. SW sends start command (enables RTC and sensors)
  3. Delay before ADC starts (i.e., MAX86141 DAC cal = ~180ms, other sensors = ~20ms)
  4. FIFO data is read periodically
  5. Every ~1s the RTC value is saved (RTC is read on FIFO interrupt)
  6. SW sends stop command
  7. The final RTC value is sent with the last FIFO sample(s)
  8. SW sends wall clock stop time (unless the device loses power before SW can send it)


Parser logic:

  1. If a start and stop wall clock timestamp are available:
    1. The RTC tick period is: (start - stop - delay)/ (final RTC value)
      1. The default delay is 180ms for MAX8614x, 20ms for other sensors, but is adjustable via a parser parameter
  2. Otherwise:
    1. The RTC tick period is (RTCscale +1)/32.768kHz
      1. Default RTCscale = 31
  3. The number of samples between two successive RTC values (which is saved every ~1s) gives the sample period for that group of samples
  4. The group of samples before the first RTC value uses (start – delay)/(number of samples before first RTC value). Hence if the delay is way off the mark, the sample period for this group will also be.
    1. It’s best to ignore the sample period for this group of samples
  5. If there isn’t a wall clock stop time (due to power loss), then the last group of samples will not have a sample period
  6. Each sample’s timestamp is the previous sample’s timestamp + its group sample period
    1. The first sample’s time stamp is the wall clock timestamp + its group sample period
Tags: MAX86171EVSYS MAXM86146EVSYS timestamp Optical AFEs format MAX86141 Optical Sensing Technology MAXM86161EVSYS MAX86140EVSYS# generation KA-13365 MAXsensorBLE MAXSENSORBLE_EVKIT MAX86141EVSYS MAX86176EVSYS MAX86140EVSYS Show More