Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    Power Management Fundamentals II Session 5: Deeper Look into Power Protection

    When is the best time to discover your power circuit needs protection? Let's explore the use of some input protection and control options like ideal diodes...
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Too Much Chatter and Not Enough Talk - Learn the Benefits...
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
    Achieving Power Over Data with RS-485 Transceivers

    By Bryson Barney What if a single wire could carry both energy and information seamlessly—without either getting in the way? The future of connectivity...

     

    ​​Functional Safety: A Driver of “Shift Left”​

    By Richard Obrien The key to faster, safer product development is to start smart - not catch up hard. In this blog, we’ll explore how the "Shift Left...

    Latest Blogs

    • The 5 Advantages of Hardware Fault Tolerance
    • The Power Problem Inside Every AI Breakthrough: Part 1 of 3
    • Simplifying Stability with EVAL-KW4503Z: Part 1 of 3
    • Energy Transfer Considerations in Isolated SMPS: Part 2 of 4
    • Automating LTspice .NOISE Measurements with .STEP and .MEAS Directives: Part 2 of 3
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
Optical Sensing Library
Optical Sensing Library
Documents How PI parameter works for HR and SpO2 algorithms?
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • -MAX86141AENP+T: FAQ
    • Are there any issues with the MAX86141 LED driver?
    • For MAX86141,Which PD and LED does maxim recommend?
    • For the HW design of MAX86141, can the Gsensor be connected to the main MCU instead of the sensor Hub MAX32664?
    • How can I use just one photodiode in the MAX86141?
    • How PI parameter works for HR and SpO2 algorithms?
    • Is there a known issue with LED current drift?
    • Maxim bio sensor algorithm takes very long time to report HR/SpO2 data.
    • Should I align the optical center of the LEDs for the wrist based SPO2 monitoring wearable design?
    • What does FDM/CDM fliter mean in MAX86141?
    • What is the requirement for algorithim to output stable SpO2 output?
    • What is the total input power requirement for the MAX86141?
    • What SPI mode does the MAX86141 use for communication?
    • Why can't the MAX86141 driver automatically adjust LED brightness after successfully porting the driver code?
    • Why we need to do calibration for SpO2 algorithm? Is it workable without calibration?
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

How PI parameter works for HR and SpO2 algorithms?

PI is one aspect of PPG signal quality. It is defined by AC/DC of PPG signal. 
The PI value varies for different subjects, diffent optical designs.
Both HR and SpO2 algorithm likes higher PI PPG signal, which means the PPG signal is more high quality, more clear.
However, if PI is good enough, saying over 0.05%, it is no longer an issue for HR algorithm. Things are different for SpO2 algorithm. SpO2 algorithm needs not only higher PI PPG signals. The higher, the better. SpO2 algorithm also need stable PI PPG signals. This is very important for stable and accurate SpO2 numbers output.

Tags: pi KA-13336 MAX86141AENP+T spo2