Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    A 16T/16R X-Band Direct Sampling Phased Array Subsystem using Apollo MxFE

    Join our webinar on the Quad Apollo Platform, a cutting-edge solution for accelerating high-performance digital beamforming. Discover the ADXBAND16EBZ...
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    ​​Where Errors Lurk in the GMSL Signal Chain​

    Whether you're debugging a stubborn camera link or designing a robust system from scratch, knowing where errors hide is half the battle. GMSL provides...

     

    Achieving Power Over Data with RS-485 Transceivers

    By Bryson Barney What if a single wire could carry both energy and information seamlessly—without either getting in the way? The future of connectivity...

    Latest Blogs

    • ​​Functional Safety: A Driver of “Shift Left”​
    • The 5 Advantages of Hardware Fault Tolerance
    • The Power Problem Inside Every AI Breakthrough: Part 1 of 3
    • Simplifying Stability with EVAL-KW4503Z: Part 1 of 3
    • Energy Transfer Considerations in Isolated SMPS: Part 2 of 4
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
Optical Sensing Library
Optical Sensing Library
Documents ​​​​​​​What is the function of 3-AXIS Sensor KX122 in MAXM86161EVSYS? Can I use other kind of 3-AXIS sensor and connect it to the I2C interface of MCU, rather than connecting it to MAX32664?
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • +MAX86141AENP+T: FAQ
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • -MAXM86161EVSYS#: FAQ
    • Can I flash the MAXM86161EVSYS with the original .msbl file v30.2.3 that is compatible with the GUI again?
    • Can I measure HRV and SPO2 by using MAXM86161 EVSYS?
    • For MAXM86161EVSYS, how to connect the OSBFLEX PCB to MAXM86161ADPTR board?
    • Is the MAXM86161 module suitable for monitoring infant heartbeats, heart rate variability, and SpO2?
    • What is the use of MAXM86161ADPTR board in MAXM86161EVSYS?
    • When I try to connect to the MAXM86161EVSYS it asks for a firmware update, is this normal?
    • Where can I find the bare metal C library for the MAXM86161?
    • ​​​​​​​What is the function of 3-AXIS Sensor KX122 in MAXM86161EVSYS? Can I use other kind of 3-AXIS sensor and connect it to the I2C interface of MCU, rather than connecting it to MAX32664?

​​​​​​​What is the function of 3-AXIS Sensor KX122 in MAXM86161EVSYS? Can I use other kind of 3-AXIS sensor and connect it to the I2C interface of MCU, rather than connecting it to MAX32664?

3-AXIS sensor (G-sensor) is used to measure acceleration. You can connect it to MAX32664C, at this time, you must choose KX122, since MAX32664C can only control KX122. If you want to choose other G-sensors, you can connect it to the host MCU.

 
Tags: MAXM86161EVSYS# KA-11780 3-AXIS sensor