Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers
    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers

    Introduction to Industrial I/O, libIIO, and Python software tools

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Evaluating Power Supplies with Different Compensation Settings

    Evaluating Power Supplies with Different Compensation Settings

Optical Sensing Library
Optical Sensing Library
Documents When I use MAXM86161 to measure HR and SpO2, Where is the best location for the sensor module?
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • +MAX86141AENP+T: FAQ
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • -MAXM86161EFD+: FAQ
    • Do activity classifier, step counter, and energy expenditure features in MAXM86161 algorithm work for in-ear applications?
    • How do you monitor sudden DC shift in the ADC value on the MAXM86161?
    • Is it necessary to use 12 layers layout for MAXM86161 design?
    • Is there any filling inside the module of the MAXM86161?
    • What are the main differences between the MAXM86161 and the MAX86160?
    • What is the purpose of the LDO present on the MAXM86161?
    • What is the purpose of the sub-DAC tag on the MAXM86161?
    • When I use MAXM86161 to measure HR and SpO2, Where is the best location for the sensor module?
    • When measuring HR and SpO2 by MAXM86161, how long it will take to obtain reliable measurement results? MAXM86161 is an in-ear product, but how is the accuracy of the result when compared with the arm?
    • Which version of the MAX32664 is compatible with the MAXM86161?
  • +MAXM86161EVSYS#: FAQ

When I use MAXM86161 to measure HR and SpO2, Where is the best location for the sensor module?

As shown in the following picture, all locations are okay, but B and D are the best according to our test. We recommend users buy MAXM86161EVSYS and do some test to find which location is the best.
Tags: MAXM86161 In-ear MAXM86161EFD+ KA-11772 Optical Sensing Technology Sensors and MEMS Show More