Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

Optical Sensing Library
Optical Sensing Library
Documents The description of MAX86150 register 0x0F is different between the datasheet and the MAX86150EVSYS GUI, why?
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • +MAX86141AENP+T: FAQ
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • -MAX86150EVSYS#: FAQ
    • Can I transfer data to a PC via a USB cable, when using the MAX86150EVSYS?
    • Can the MAX86150EVSYS turn on if the battery is not connected?
    • Could you please recommend or suggest a device simulator (ECG/PPG/Spo2) for handheld medical devices to check the reliability and accuracy of the MAX86150 in our device?
    • How are the ECG TP1 and TP2 contacts in MAX86150EVSYS# constructed?
    • How do you turn off the MAX86150EVSYS?
    • How to reduce the ECG noise signals on MAX86150 Evaluation Kit?
    • In the MAX86150EVSYS# layout, what are the traces running parallel to the TP1 and TP2 traces?
    • Is Bluetooth protocol implemented in MAX86150EVSYS Bluetooth classic or BLE?
    • Is the filter library source code available for the MAX86150EVSYS
    • Is there any provision to change the ECG sampling rate of MAX86150EVSYS?
    • Is there any sequence to set parameters to MAX86150?
    • The description of MAX86150 register 0x0F is different between the datasheet and the MAX86150EVSYS GUI, why?
    • What batteries can be used with the MAX86150EVSYS?
    • What to do for MAX86150EVSYS, the Red LED is blinking but the Blue LED is not
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

The description of MAX86150 register 0x0F is different between the datasheet and the MAX86150EVSYS GUI, why?

Revision Creation Date Revision Author
Current Revision 10 Feb 2026 10:41 PM EngineerZone
Revision #4 10 Feb 2026 5:58 PM MSDAPI
Revision #3 10 Feb 2026 5:58 PM MSDAPI
Revision #2 19 Dec 2023 6:35 PM MSDAPI
Revision #1 17 Jun 2020 8:52 AM MSDAPI
  • Compare Versions View current version