Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    This webinar will introduce remote-controlled edge nodes and how they promise to simplify the automotive network architecture and expedite the integration...
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
      1. Quote of the week: "Knowledge is knowing a tomato is a fruit. Wisdom is not putting it in a fruit salad" - unknown Sources: commons.wikimedia...

    View All

    What's Brewing

      GMSL Quiz! Read the blog, take the quiz, and enter to win a gift card!

      Quiz! Read the GMSL Link Lock Blog - Take the Quiz and You are Entered to Win! Important: Read the blog first . The quiz questions are all based on...
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
    The Limitation of Heat Dissipation IO-Link is used across many branches of factory automation, and in these applications, areas of the factory floor...

     

    GMSL Debugging: Getting a Lock

    Imagine a scenario where you have a brand-new board design or are excited to try out some evaluation kits only to find out that the two devices can’t talk...
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
Optical Sensing Library
Optical Sensing Library
Documents Are larger currents better for the MAX30101 luminous tube?
  • File Uploads
  • Documents
  • Members
  • Tags
  • More
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • -MAX30101EFD+_T1: FAQ
    • Are larger currents better for the MAX30101 luminous tube?
    • Can a single crystal oscillator be shared between multiple ICs ?
    • Can MAX30101 be used to measure the respiratory rate?
    • Can the luminous intensity of the MAX30101 LED be independently adjusted?
    • Can the MAX30101/MAX30102 detect when the medical device is no longer attached?
    • Can the systolic blood pressure be obtained from the PPG and ECG signals?
    • Does Maxim offer Algorithm of SpO2 and HR Calculation in PPG solution?
    • Does the MAX30101 requires temperature compensation?
    • For the MAX30101 in HR mode (no green LED) is it acceptable to power the VLED from an unregulated source such as a Li-ion battery (3.0-4.2V)?
    • How can we stop the MAX30101 from collecting data without disrupting the communication or resetting the registers?
    • How to avoid water condensation inside the MAX30101/5?
    • How to minimize error due to the self-heating effect of the LED’s in the MAX30101?
    • In Multi-LED mode, if SLOTx in the MAX30101 is disabled will I receive dummy bytes?
    • Is it possible to relocate the three electrodes from the chest to the human body backside for BioZ?
    • Is it recommended to use two green LEDs for heart rate measurement using the wrist?
    • Is the SLOTx[2:0] 000b value in the Multi-LED Mode Control Registers the same as 100b for the MAX30101/2?
    • Is there a way to change the I2C address of the MAX30101 or MAX30102?
    • Is there any wake up delay after toggling the SHDN bit in the MAX30101?
    • Is there minimum requirement for the cover glass thickness of MAX30101?
    • Questions on application note 6547
    • The measured waveforms from the MAX30101 and MAX30102 do not match the standard waveforms on the web. Why is this?
    • What are the optimal current values for the LEDs in the MAX30101 for wrist-based biosensor measurements?
    • What is an OHR solution?
    • What is the order of sample data output from the MAX30101?
    • What is the recommended connection of pins 5, 6, 7 in the MAX30101?
    • What is the saturation value of the MAX30101 OVF_COUNTER register?
    • What should be the spectral response of the cover window material for the MAX30101?
    • What value does the MAX30101 FIFO_A_FULL register represent?
    • Why does quality of the HR and SpO2 reading from the MAX30101 decrease when my finger is cold?
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • +MAX86141AENP+T: FAQ
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

Are larger currents better for the MAX30101 luminous tube?

Considering power consumption and effective resolution, it is not better to have a larger current. However, for some parts to be measured (such as a wrist), or objects to be measured (such as people with darker skin color and people who are physically overweight), the current of the luminous tube needs to be increase to effectively obtain the strength of the available signal and obtain the measured value.

Tags: MAX30101EFD+ KA-09699