Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    Power Management Fundamentals II Session 6: Key Layout Considerations for Power

    Understand the physics of printed circuit boards to manage large changes in current or voltage. See how layout tweaks can make big improvements for your...
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
    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3

    Noise analysis of a circuit requires tracking several things simultaneously: each noise source, how those noise sources are shaped by the circuit, and...

     

    ​​Where Errors Lurk in the GMSL Signal Chain​

    Whether you're debugging a stubborn camera link or designing a robust system from scratch, knowing where errors hide is half the battle. GMSL provides...

    Latest Blogs

    • Achieving Power Over Data with RS-485 Transceivers
    • ​​Functional Safety: A Driver of “Shift Left”​
    • The 5 Advantages of Hardware Fault Tolerance
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
Optical Sensing Library
Optical Sensing Library
Documents Maxim bio sensor algorithm takes very long time to report HR/SpO2 data.
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • -MAX86141AENP+T: FAQ
    • Are there any issues with the MAX86141 LED driver?
    • For MAX86141,Which PD and LED does maxim recommend?
    • For the HW design of MAX86141, can the Gsensor be connected to the main MCU instead of the sensor Hub MAX32664?
    • How can I use just one photodiode in the MAX86141?
    • How PI parameter works for HR and SpO2 algorithms?
    • Is there a known issue with LED current drift?
    • Maxim bio sensor algorithm takes very long time to report HR/SpO2 data.
    • Should I align the optical center of the LEDs for the wrist based SPO2 monitoring wearable design?
    • What does FDM/CDM fliter mean in MAX86141?
    • What is the requirement for algorithim to output stable SpO2 output?
    • What is the total input power requirement for the MAX86141?
    • What SPI mode does the MAX86141 use for communication?
    • Why can't the MAX86141 driver automatically adjust LED brightness after successfully porting the driver code?
    • Why we need to do calibration for SpO2 algorithm? Is it workable without calibration?
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

Maxim bio sensor algorithm takes very long time to report HR/SpO2 data.

Maxim algorithm v1.9.3 needs around 20s-30s to get HR numbers. For SpO2, it costs around 45s if signal quality is good.
Our algorithm team has plan to shorten that and will release new version later. We also could do some smart operations in the application layer: report the numbers earlier when the confidence level is low. And gradually converge to more reliable numbers.

Tags: MAX86141AENP+ KA-09441 MAX86141 algorithem