Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    View All Webinars
  • Community Hub

    Challenge Yourself!

      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

Optical Sensing Library
Optical Sensing Library
Documents Why does the PPG waveform observed through AFEs differ slightly from the PPG waveform found in medical texts?
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • -MAX30102EFD+T: FAQ
    • After setting the Mode configuration register of MAX30101/MAX30102 to be 0x03, the Mode configuration alternates between 0x03 and 0x00 when the register is read. What might be the cause of this?
    • Are the LEDs in the MAX30102 homogeneously transmitting light to the users skin, or is the transmission angle tapered internally?
    • Can MAX30102 be used for non invasive blood glucose monitoring?
    • Can MAX30102's internal temperature sensor be used to measure body temperature?
    • Can MAX30102's VLED+ run on 3.0 volts? Can VDDIO be 3 volts or does it need to be shifted down?
    • Can the IR sensor of the MAX30102 be used to measure body temperature?
    • Can you suggest any tester/simulator model for the MAX30102?
    • Disabling Digital Noise Cancellation Filter in MAX30102?
    • Does MAX30102 require an extra cover glass? If we add one, what are the requirements?
    • Does MAX30102 sample data while its FIFO is read?
    • Does the MAX30102 have an R-curve associated with it to correlate the ratio R = (ACred/DCred)/(ACir/DCir)?
    • Does the MAX30102 support I2C rapid communication mode?
    • Has the MAX30101/MAX30102 been tested for biocompatibility?
    • How can I get MAX30102 EVKit software including SKA and PBA algorithms source code?
    • How do I use the shutdown (SHDN) function of MAX30102?
    • How do the algorithms used with the MAX30102 determine heart rate from the ADC data?
    • How to control the sample rate for heart rate mode in MAX30102?
    • Is the MAX30102 hermetically sealed
    • MAX30102 Averaging Information
    • The MAX30102ACCEVKIT GUI keeps crashing while trying to find the pba.dll file, but it is installed correctly, what could be the issue?
    • Unregulated Power Source to VLED+
    • What areas of the body are popular for measuring heart rate and SpO2?
    • What is related to the data interruption of the MAX30102?
    • What is the effective noise free resolution of the MAX30102?
    • What is the maximum altitude specification for the MAX30102?
    • What is the purpose of the R_DRV and IR_DRV in MAX30101/MAX30102? How do I connect them?
    • What is the reason behind Random Spikes on MAX30102 ?
    • What should be the spectral response of the cover window material for the MAX30102?
    • What's your recommendation on bio sensor parts for mobile phone application? Should we use AFE parts ?
    • Where is the MAX30102 shutdown mode supply current?
    • While using MAX30102, if mode = 010 or heart rate mode, is one full sample 3 bytes only?
    • Why does the PPG waveform observed through AFEs differ slightly from the PPG waveform found in medical texts?
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • +MAX86141AENP+T: FAQ
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

Why does the PPG waveform observed through AFEs differ slightly from the PPG waveform found in medical texts?

PPG AFEs measure the PPG signal via the intensity of the light reflected into photodiodes, and as the blood volume in the arteries increases, following the contraction during the systolic phase, so does the absorption of the light being shined into the tissue. Since there is more absorption, the photodiodes will receive less reflected light and the output of the AFE will decrease. During the diastolic phase, while there is less blood in the arteries there will be less absorption and therefore more reflected light to the photodiodes. Hence the output of the PPG AFEs is just an inversion of the PPG plot that you find in medical texts.

 

 

Tags: KA-09386 MAX30102EFD+ ppg AFEs MAX30102