Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    Join us for an in-depth webinar where we dive into the world of EMC testing applied to ADI’s digital isolators. We''ll walk through the test setups, standards...
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
      1. First, the quote of the week: " The best measure of a man's honesty isn't his income tax return. It's the zero adjust on his bathroom scale " - Unknown...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: White Coats and Multi-Coloured Pens Ready to put...
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
    What happens when your system needs to talk across noisy or high-voltage boundaries? Isolation steps in. In a previous blog post, we discussed the fundamentals...

     

    Understanding Safe Failure Fraction: Can There Be Multiple Values?

    I discuss various aspects of the SFF (safe failure fraction) —whether it applies to an integrated circuit —and whether an integrated circuit can have more...
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
Optical Sensing Library
Optical Sensing Library
Documents For the HW design of MAX86141, can the Gsensor be connected to the main MCU instead of the sensor Hub MAX32664?
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • -MAX86141AENP+T: FAQ
    • Are there any issues with the MAX86141 LED driver?
    • For MAX86141,Which PD and LED does maxim recommend?
    • For the HW design of MAX86141, can the Gsensor be connected to the main MCU instead of the sensor Hub MAX32664?
    • How can I use just one photodiode in the MAX86141?
    • How PI parameter works for HR and SpO2 algorithms?
    • Is there a known issue with LED current drift?
    • Maxim bio sensor algorithm takes very long time to report HR/SpO2 data.
    • Should I align the optical center of the LEDs for the wrist based SPO2 monitoring wearable design?
    • What does FDM/CDM fliter mean in MAX86141?
    • What is the requirement for algorithim to output stable SpO2 output?
    • What is the total input power requirement for the MAX86141?
    • What SPI mode does the MAX86141 use for communication?
    • Why can't the MAX86141 driver automatically adjust LED brightness after successfully porting the driver code?
    • Why we need to do calibration for SpO2 algorithm? Is it workable without calibration?
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

For the HW design of MAX86141, can the Gsensor be connected to the main MCU instead of the sensor Hub MAX32664?

Revision Creation Date Revision Author
Current Revision 19 Dec 2023 6:13 PM MSDAPI
Revision #1 7 Dec 2019 2:57 PM MSDAPI
  • Compare Versions View current version