Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

Optical Sensing Library
Optical Sensing Library
Documents For the HW design of MAX86141, can the Gsensor be connected to the main MCU instead of the sensor Hub MAX32664?
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • -MAX86141AENP+T: FAQ
    • Are there any issues with the MAX86141 LED driver?
    • For MAX86141,Which PD and LED does maxim recommend?
    • For the HW design of MAX86141, can the Gsensor be connected to the main MCU instead of the sensor Hub MAX32664?
    • How can I use just one photodiode in the MAX86141?
    • How PI parameter works for HR and SpO2 algorithms?
    • Is there a known issue with LED current drift?
    • Maxim bio sensor algorithm takes very long time to report HR/SpO2 data.
    • Should I align the optical center of the LEDs for the wrist based SPO2 monitoring wearable design?
    • What does FDM/CDM fliter mean in MAX86141?
    • What is the requirement for algorithim to output stable SpO2 output?
    • What is the total input power requirement for the MAX86141?
    • What SPI mode does the MAX86141 use for communication?
    • Why can't the MAX86141 driver automatically adjust LED brightness after successfully porting the driver code?
    • Why we need to do calibration for SpO2 algorithm? Is it workable without calibration?
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

For the HW design of MAX86141, can the Gsensor be connected to the main MCU instead of the sensor Hub MAX32664?

 

The Gsensor can be connected to the main MCU or the sensor Hub MAX32664, but the following points should be noted,

1. The Gsensor is connected to the main MCU and can read the data directly when it is used for step counting and other applications, so the MAX32664 does not need to transfer the data, so it saves more power.

2. Gsensor is connected to the Sensor Hub MAX32664. For HR and Spo2, Gsensor and BIO Sensor have better synchronization, which is more conducive to algorithm processing.

 

Tags: MAX86141AENP+ Optical AFEs Gsensor MAX86141 Optical Sensing Technology KA-08465 Sensor Hubs max32664 Processors and Microcontrollers MAX86171 Show More