Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Fast-Track Certification: Leveraging IC Safety App Notes for Functional Safety Designs
    View All Webinars
  • Community Hub

    Challenge Yourself!

      World Engineering Day Quiz!

      By Kuo-Chang A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

Optical Sensing Library
Optical Sensing Library
Documents What Bluetooth dongle is compatible with the MAX86140EVSYS?
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • -MAX86140EVSYS#: FAQ
    • After installing the software by following the procedure in the evkit datasheet, I can see the COM port . However, there is no response after pressing "connect," and the MAX86140EVSYS cannot be connected. Why is that?
    • Error Message "Unable to load DLL 'PSnrACDC.dll': The specified module could not be found." while launching software
    • How does the timestamp is formatted and generated on the MAXSENSORBLE_EVKIT board for the some of the PPG sensor's Evaluation Kits?
    • How to upgrade MAXSensorBLE F/W using the MRD100HDK
    • In the MAX86140EVSYS, do you use a standard heart rate service defined by the SIG or it is a custom service with custom characteristics? and which Bluetooth version is implemented?
    • What battery is recommended for use with the MAX86140EVSYS?
    • What Bluetooth dongle is compatible with the MAX86140EVSYS?
    • Which are the available dongles required for the MAX86140EVSYS?
    • Why I can not run the MAX86140EVSYS on my Windows 7 Operating system?
    • Why is MAX86140EVSYS GUI PPG Plot Data Information not showing PSNR, PSNR Avg, AC, DC?
  • MAX86141AENP+: FAQ
  • +MAX86141AENP+T: FAQ
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

What Bluetooth dongle is compatible with the MAX86140EVSYS?

Revision Creation Date Revision Author
Current Revision 10 Feb 2026 11:29 AM MSDAPI
Revision #4 10 Feb 2026 11:29 AM MSDAPI
Revision #3 22 Jan 2025 12:44 PM MSDAPI
Revision #2 19 Dec 2023 6:02 PM MSDAPI
Revision #1 29 Aug 2019 3:17 PM MSDAPI
  • Compare Versions View current version