Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Calibration Implementation Techniques for Multichannel Phased Array Subsystems

    Learn about phase-calibration techniques used for characterizing a 16 transmit and 16 receive X-band phased array subsystem based on a mixed-signal front...

Optical Sensing Library
Optical Sensing Library
Documents What to do for MAX86150EVSYS, the Red LED is blinking but the Blue LED is not
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • +MAX86141AENP+T: FAQ
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • -MAX86150EVSYS#: FAQ
    • Can I transfer data to a PC via a USB cable, when using the MAX86150EVSYS?
    • Can the MAX86150EVSYS turn on if the battery is not connected?
    • Could you please recommend or suggest a device simulator (ECG/PPG/Spo2) for handheld medical devices to check the reliability and accuracy of the MAX86150 in our device?
    • How are the ECG TP1 and TP2 contacts in MAX86150EVSYS# constructed?
    • How do you turn off the MAX86150EVSYS?
    • How to reduce the ECG noise signals on MAX86150 Evaluation Kit?
    • In the MAX86150EVSYS# layout, what are the traces running parallel to the TP1 and TP2 traces?
    • Is Bluetooth protocol implemented in MAX86150EVSYS Bluetooth classic or BLE?
    • Is the filter library source code available for the MAX86150EVSYS
    • Is there any provision to change the ECG sampling rate of MAX86150EVSYS?
    • Is there any sequence to set parameters to MAX86150?
    • The description of MAX86150 register 0x0F is different between the datasheet and the MAX86150EVSYS GUI, why?
    • What batteries can be used with the MAX86150EVSYS?
    • What to do for MAX86150EVSYS, the Red LED is blinking but the Blue LED is not
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

What to do for MAX86150EVSYS, the Red LED is blinking but the Blue LED is not

The Blue LED will blink only after paring the EVSYS with Bluetooth. Red LED will initially blink which means ready to pair but not paired with the EVSYS

Tags: MAX86150EVSYS# MAX86150EVSYS KA-06929