Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

Optical Sensing Library
Optical Sensing Library
Documents Which Maxim SpO2 chips can be used in transmissive pulse oximetry?
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • -MAX86140ENP+: FAQ
    • Can the MAX86140 and MAX30205 be used for monitoring farm animals?
    • Can you recommend a LED and photodiode compatible with the MAX86140/86141?
    • For high precision measurement where should VDDANA be connected?
    • IEC-62471 documentation for MAX86140
    • Is there any cover glass in MAX86140/86141?
    • MAX86140如何测试环境光的范围和抑制比
    • VDDANA of MAX86141
    • Which Maxim SpO2 chips can be used in transmissive pulse oximetry?
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • +MAX86141AENP+T: FAQ
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

Which Maxim SpO2 chips can be used in transmissive pulse oximetry?

The MAX30110, the MAX86140 and the MAX86141 can be used to measure SpO2 by transmissive means.  
    
There are two methods of pulse oximetry measurement.  The first is when certain wavelengths of light are transmitted through, say, a fingertip or earlobe, and the amount of light absorption changes caused by arterial blood flow pulsations is detected and measured on the other side.  This is "transmissive" pulse oximetry.  The other method of pulse oximetry is called "reflectance".  This method has the light transmitter and receiver in the same plane. 
    
While most of Maxim's first generation of pulse oximetry devices are designed with reflective pulse oximetry in mind, the MAX30110 is the better choice for transmissive designs.  For Maxim's second generation of pulse oximetry devices with ultra-low power consumption, the MAX86140 and MAX86141 are well-suited for transmissive designs.

 

Tags: pulse Optical AFEs MAX86140ENP+ MAX30110 MAX86141 Optical Sensing Technology MAX86140 oximeter KA-02547 transmissive oximetry spo2 Show More