Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

Optical Sensing Library
Optical Sensing Library
Documents MAX30102 Averaging Information
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • -MAX30102EFD+T: FAQ
    • After setting the Mode configuration register of MAX30101/MAX30102 to be 0x03, the Mode configuration alternates between 0x03 and 0x00 when the register is read. What might be the cause of this?
    • Are the LEDs in the MAX30102 homogeneously transmitting light to the users skin, or is the transmission angle tapered internally?
    • Can MAX30102 be used for non invasive blood glucose monitoring?
    • Can MAX30102's internal temperature sensor be used to measure body temperature?
    • Can MAX30102's VLED+ run on 3.0 volts? Can VDDIO be 3 volts or does it need to be shifted down?
    • Can the IR sensor of the MAX30102 be used to measure body temperature?
    • Can you suggest any tester/simulator model for the MAX30102?
    • Disabling Digital Noise Cancellation Filter in MAX30102?
    • Does MAX30102 require an extra cover glass? If we add one, what are the requirements?
    • Does MAX30102 sample data while its FIFO is read?
    • Does the MAX30102 have an R-curve associated with it to correlate the ratio R = (ACred/DCred)/(ACir/DCir)?
    • Does the MAX30102 support I2C rapid communication mode?
    • Has the MAX30101/MAX30102 been tested for biocompatibility?
    • How can I get MAX30102 EVKit software including SKA and PBA algorithms source code?
    • How do I use the shutdown (SHDN) function of MAX30102?
    • How do the algorithms used with the MAX30102 determine heart rate from the ADC data?
    • How to control the sample rate for heart rate mode in MAX30102?
    • Is the MAX30102 hermetically sealed
    • MAX30102 Averaging Information
    • The MAX30102ACCEVKIT GUI keeps crashing while trying to find the pba.dll file, but it is installed correctly, what could be the issue?
    • Unregulated Power Source to VLED+
    • What areas of the body are popular for measuring heart rate and SpO2?
    • What is related to the data interruption of the MAX30102?
    • What is the effective noise free resolution of the MAX30102?
    • What is the maximum altitude specification for the MAX30102?
    • What is the purpose of the R_DRV and IR_DRV in MAX30101/MAX30102? How do I connect them?
    • What is the reason behind Random Spikes on MAX30102 ?
    • What should be the spectral response of the cover window material for the MAX30102?
    • What's your recommendation on bio sensor parts for mobile phone application? Should we use AFE parts ?
    • Where is the MAX30102 shutdown mode supply current?
    • While using MAX30102, if mode = 010 or heart rate mode, is one full sample 3 bytes only?
    • Why does the PPG waveform observed through AFEs differ slightly from the PPG waveform found in medical texts?
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • +MAX86141AENP+T: FAQ
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

MAX30102 Averaging Information

Question: If mode = 011 or SpO2, there are 2 sets of data (Red and IR) for one full sample. If SMP_AVE[2:0] > 0 in register 0x08, does the averaging number applies to individual channel independently?

Answer: If SMP_AVE[2:0] > 0 in register 0x08,  the averaging number does indeed apply to individual channel independently.

Tags: KA-01187 Optical AFEs MAX30102EFD+ averaging Optical Sensing Technology Individual Channel MAX30102 Show More