Answer:
No, the photodiode is optimized for the spectrum of the LEDs used. (The IR LED is 880 nm; the red LED is 660 nm.) Measuring body temperature requires a good response to wavelengths more than 10 times longer, which is not feasible using a silicon photodiode. If non-contact temperature measurement is required then a thermopile-based sensor would be better suited.