Bits 3:0: FIFO Almost Full Value (FIFO_A_FULL)
This register sets the trigger for the FIFO_A_FULL interrupt. For example, if set to 0x0F, the interrupt triggers when there are 15 empty spaces left (17 data samples), and so on.| FIFO_A_FULL[3:0] | NO. OF SAMPLES IN THE FIFO |
|---|---|
| 0x00h | 32 |
| 0x01h | 31 |
| 0x02h | 30 |
| 0x03h | 29 |
| .. | .. |
| 0x0Fh | 17 |