Why is the MAX30101_xxxxx.csv missing HR and SpO2 samples when using the eval kit GUI?
Please ignore the MAX30101_xxxxx.csv file as the data in this file is incomplete. There is currently no schedule as to when this will be fixed. Instead, please use the dataset from MAX30101_xxxx_PPG.csv and MAX30101_xxxx_XYZ.csv. SpO2 and heart rate can be calculated by post processing the PPG log in the csv files.