Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
  • Forums

    Popular Forums

    • LTspice
    • RF and Microwave
    • Video
    • Power Management
    • Precision ADCs
    • FPGA Reference Designs
    • Linux Software Drivers

    Product Forums

    • Amplifiers
    • Microcontrollers
    • Clock and Timing
    • Data Converters
    • Direct Digital Synthesis (DDS)
    • Energy Monitoring and Metering
    • Interface and Isolation
    • MEMS Inertial Sensors
    • Power Management
    • Processors and DSP
    • Switches/Multiplexers
    • Temperature Sensors
    • Voltage References
    View All

    Application Forums

    • A2B
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
    • Design Tools and Calculators
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
    Maximize Your Power Regulator: Key Considerations for Thermal Performance

    Power regulators with integrated switches deliver a compact, efficient way to supply power. Yet as modern circuits drive toward ever-higher power densities...
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
    • Maximize Your Power Regulator: Key Considerations for Thermal Performance
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quizzes AQQ295 about an audio logarithmic volume controller using linear pot - a proposal from Tim O'Brien

      1. Quote of the month: "Think like a proton. Always positive" - Unknown 2. New quiz of the month: AQQ295 about a audio logarithmic volume controller...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Let's Take a Field-Bus Trip Your field-bus engines...
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
    Understanding Voltage Domain Isolation in Field-Bus Systems

    By Christopher Nunes In the world of industrial communication, mastering voltage domain isolation is the key to building safer, smarter systems. Last...

     

    Ethernet-APL’s Impact on Functional, Intrinsic, and Cyber Safety

    Power limitations have always plagued process sensors, whether because of intrinsic safety requirements (safety achieved through power limitation) or because...

    Latest Blogs

    • Balancing Enhanced Radar Resolution with FPGA-Based Pulse Compression
    • ​​ISO 26262 Essentials: Ensuring Confidence in Your Software Tools ​
    • Step-by-Step: Implementing a Complete DSP Chain for Signal Analysis
    • Galvanic Isolation in SMPS: Ensuring Safety and Protection: Part 1 of 4
    • Mature, Not Old! The Longevity of 4 – 20 mA
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
Optical Sensing Library
Optical Sensing Library
Documents How do I set the sample rate for SpO2 measurements in multi-LED mode for the MAX30101?
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • -MAX30101ACCEVKIT#: FAQ
    • After unzipping the file "MAX30101ACCEVKIT_PCBA.ZIP" I could not find the Gerber files. Can you please advise?
    • Are there recommendations for power sequencing, isolation, and temperature management for the MAX30101/2?
    • Can 3.3V logic be used for the I2C pins of the MAX30101 even though VDD is 1.8V?
    • Can Maxim provide the MAX30101 LED location and package details?
    • Can the IR sensor of the MAX30101 be used to measure body temperature?
    • For MAX30101, is it necessary to add extra light barrier between chip glass and phone glass?
    • How can a customer package a MAX30101 to be used underwater?
    • How can PPG signal quality be improved when measured on the wrist?
    • How do I configure MAX30101 in Multi-LED Mode?
    • How do I convert the "Time" output in the log output by the MAX30101ACCEVKIT into seconds?
    • How do I read the FIFO of MAX30101?
    • How do I set the sample rate for SpO2 measurements in multi-LED mode for the MAX30101?
    • How do I set up interrupt for MAX30101/MAX30102 for reading data?
    • How to select the green LED only on the MAX30101
    • If I enable sample averaging in MAX30101/MAX30102 and keep the sampling rate setting to be the same, does the effective sampling rate go down?
    • In PPG monitor, is Yellow LED used and what is the advantage?
    • Is it possible to directly use the daughter board (MAX30101DBEVKIT) with an alternate microcontroller for evaluation, without connecting to the motherboard (USBOSMB)?
    • MAX30101 UV tolerant?
    • What are the factors that makes impact on the time delay between AFE conversion start time and  PPG Data Ready ?
    • What Cover Material Can I Use for the MAX30101, MAX30102, or MAX30105?
    • What is the sampling rate assumed in the PBA algorithm provided for the MAX301xx optical sensors?
    • Which Maxim Pulse Oximeters integrate Red/IR LEDs?
    • Why do the green and red LEDs on the mother board keep flashing, when using the MAX30101ACCEVKIT?
    • Why is the MAX30101 green LED not lighting?
    • Why is the PPG signal saturated when using the MAX30101, MAX30102, or MAX30105?
    • Why is the time taken for an initial result of HR and SpO2 different ?
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • +MAX30102ACCEVKIT#: FAQ
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • +MAX86141AENP+T: FAQ
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

How do I set the sample rate for SpO2 measurements in multi-LED mode for the MAX30101?


You do this in the same way as the other modes.  This is because in multi-LED mode, a sample consists of three slots, one for each LED.  To set the sample rate, the user has to write to the bits [4:2] of the SpO2 Configuration register with address 0x0Ah.  Table 6 in the datasheet lists the available samples-per-second configurations.
 
Tags: optical sensing 000094529 max30101
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
©2025 Analog Devices, Inc. All Rights Reserved
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
©2025 Analog Devices, Inc. All Rights Reserved