Locale Icon
English
EngineerZone
EngineerZone
Optical Sensing Library
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
    Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

Optical Sensing Library
Optical Sensing Library
Documents What Prevents "USB HID Report Timeout" Errors with the MAX30102ACCEVKIT?
  • File Uploads
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ADN8831: FAQ
  • +ADN8834: FAQ
  • +ADN8835: FAQ
  • +ADPD1080: FAQ
  • +ADPD1081: FAQ
  • +ADPD144RI: FAQ
  • +ADPD188BI: FAQ
  • +ADPD2140: FAQ
  • MAX1968: FAQ
  • +MAX1968EUI: FAQ
  • +MAX1968EVKIT: FAQ
  • +MAX1978ETM+: FAQ
  • +MAX1978EVKIT+: FAQ
  • +MAX1979: FAQ
  • +MAX30005CTI+: FAQ
  • +MAX30101ACCEVKIT#: FAQ
  • MAX30101ACCEVKIT: FAQ
  • +MAX30101DBEVKIT#_T1: FAQ
  • MAX30101EFD+: FAQ
  • +MAX30101EFD+_T1: FAQ
  • -MAX30102ACCEVKIT#: FAQ
    • Is there Software for the MAX30102ACCEVKIT that runs on Mac OS?
    • What is the difference between the MAX30101ACCEVKIT# and MAX30102ACCEVKIT#?
    • What Prevents "USB HID Report Timeout" Errors with the MAX30102ACCEVKIT?
    • When I use the MAX30102EVKIT software, it crashes due to a pba.dll error. How do I fix this?
    • Why is the MAX30101_xxxxx.csv missing HR and SpO2 samples when using the eval kit GUI?
    • Why is the message "HR/SPO2 only valid for Fs=100Sps" displayed in the MAX30102ACCEVKIT GUI?
    • Why is the VLED+ voltage on the MAX30102ACCEVKIT at 4.4V?
  • MAX30102ACCEVKIT: FAQ
  • MAX30102EFD+: FAQ
  • +MAX30102EFD+T: FAQ
  • +MAX30110ACCEVKIT#: FAQ
  • +MAX30112EWG+: FAQ
  • +MAX8521ETP+: FAQ
  • +MAX8521EWX+: FAQ
  • +MAX86140AENP+: FAQ
  • +MAX86140ENP+: FAQ
  • +MAX86140EVSYS#: FAQ
  • MAX86141AENP+: FAQ
  • +MAX86141AENP+T: FAQ
  • +MAX86141ENP+T: FAQ
  • +MAX86141ENP+_B1: FAQ
  • +MAX86150EFF+: FAQ
  • +MAX86150EVSYS#: FAQ
  • +MAX86170BENG+T: FAQ
  • MAX86171ENI+: FAQ
  • +MAX86171ENI+T: FAQ
  • +MAX86171EVSYS#: FAQ
  • +MAX86176ENX+T: FAQ
  • +MAX86176EVSYS#: FAQ
  • +MAX86916EFD+: FAQ
  • +MAXM86146CFU+: FAQ
  • +MAXM86146EVSYS#: FAQ
  • +MAXM86161EFD+: FAQ
  • +MAXM86161EVSYS#: FAQ

What Prevents "USB HID Report Timeout" Errors with the MAX30102ACCEVKIT?

See below for a screenshot of the MAX30102ACCEVKIT# software GUI's error prompt with the text "USB HID report timeout; no interrupt?  Board power? I2C connection?"



This error is typically due to incorrect connection of the flexible cable between the microcontroller board and the sensor.  Here are two photographs showing proper orientation:



The customer should carefully reconnect the two boards with the flexible ribbon cable, keeping in mind two things:
1) A little more force than originally expected may be required to get the cable into the connectors to where they make good electrical connection.
2) The cabling is small, and thus it is very easy to connect to the boards incorrectly -- such as attaching the cable at an angle, upside down, or not all the way in, etc. These conditions generate the above USB HID errors specifically when the GUI has found the microcontroller but is unable to communicate with the sensor.

 
Tags: MAX30102ACCEVKIT# 000094436