Post Go back to editing

ADPD105 FIFO data packet format

What is the data format of the samples stored in the FIFO for both slots enabled (same ODR) and 32-bit mode?

I haven't been able to decipher the format of the data stored in the FIFO from the datasheet or code examples.  Attached is the configuration I am using for the WaveTool and a saved configuration. 

A detailed description of the FIFO data packet format (data packet is the terminology used on pg 33. of the datasheet RevA) for 16-bit and 32-bit configurations would be useful.  The configuration below is for 32-bit, 4 channels.

Are the samples stored in the FIFO big endian?  Are the sample stored in slot A: channels 1,2,3,4, then slot B: channels 1,2,3,4?  Or is the format similar to registers 0x70-0x7F?

attachments.zip