ADPD1080 32MHz clock

Hi ADI Engineers!

Updates:

W 0x2680 to 0x4B, R back to verify: 0x2680

W 0x0001 to 0x01,    R : 0x0001 : Prog mode

W 0x303A to 0x23,   R:  0x303A

W 0x0A20 to 0x30,   R:  0x0A20

W 0x0826 to 0x31,   R:  0x0826

W 0x5AFC to 0x39,   R:  0x5AFC

W 0x0001 to 0x5F,   R:  0x0001 : turning on the 32MHz clock

W 0x0020 to 0x50,   R  0x0020 : starting 32MHz clock calibration 

Then Read  0x0A.  got  0x052D (==1325)  -->  32MHz clock running

W 0x0000 to 0x5F,  R:  0x0000 : turning off 32MHz clock

W 0x00E07 to 0x0B,  R:  0x0E07 : sending  pulses to GPIO

W 0x0002 to 0x10,  R:  0x0002 : jumping to run mode

Checked GPIO0, GPIO1, and LED's circuit on oscilloscope: still NO pulses ---> 32MHz running????

Mistakes in my Regs settings or a bad Eval board?

I connected the ADPD1080 Eval board to my ESP-32 WRover to work with, (on ESP-IDF/Eclipse.) The ESP-32 board has working BLE, COM, WebSocket  and CAN bus to bridge PC to EFI devices. Now I'm trying to add I2S interface for the ADPD1080 and get stuck. I could write then read back registers' values while programming them, but could not send out any pulses to the IR LEDs' as expected. What were wrong. I set wrong values for regs, missed some settings, or set pulse rate to high, or worst case, the ADPD board was bad?

Should I first get and try an AD controller board instead of using my own one? The problem is I don't know if I will have control/access on the code of the AD controller board?

Thanks for every Idea.

KNguyen



Back to work on this project this week June 7th, 2021 with more info.
[edited by: Knguyen at 7:58 PM (GMT -4) on 8 Jun 2021]