I'm trying to connect two photo diodes for channel 1-2 and channel 3-4 on the ADPD105 Eval Board
On P3 I used
pin 1 for common cathode
pin 2 for channel 3-4 anode first photo diode
pin 3 for channel 1-2 anode second photo diode
and of course I removed jumper on P7 to disable the onboard photo diode.
Using the APDP OpenMarket Wave Tool 1.0.11.1 the channels 1 and 2 are constantly "0".
I already did an cross check and swapped the photo diodes on pin 2 and 3. Again I see the signal only on channel 3 and 4. So I am sure both photo diodes deliver a signal, but I only see values for channel 3 and 4.
Time Slot Switch (Register 0x14)
SLOTB_PD_SEL: 0x5: PD1-2 is connected to Channel 1 and Channel 2; PD3-4 is connected to Channel 3 and Channel 4 during Time Slot B.
SLOTA_PD_SEL: 0x5: PD1-2 is connected to Channel 1 and Channel 2; PD3-4 is connected to Channel 3 and Channel 4 during Time Slot A.
Any idea, why I don't see a signal in channel 1 and 2 in the APDP OpenMarket Wave Tool?
Many Thanks
Peter