Working with Avalanche photo diode - Beginner problems

i have avalanche photo diode with which i am trying to digitalize the current from TIA through a comparator, the diode biased using a HVDCDC

the source is being a 20ns laser with a PRF of 3Khz

the circuit is as below

 

I understand that the IC is LT's but i want some light from Analog as well, as its part of you now

 

the output of opamp for an high intensity light is like above, we can see the opamp fully saturated, but i am clue less about the over shoot and ringing effect, this happened when i have put my bias voltage 300V, i am not able to stop the opamp to enter in to saturation.

even if i see the datasheet of DC-DC CA05N, it can maximum source 2mA of current, and the peak current of didoe is only 0.25mA, so i understood the dcdc current is exceeding 2mA

so to avoid the opamp going in to saturation i tried to use a 300K in series with the source but still the opamp went to saturation,

it evident that in order to make the opamp not to go in to saturation, the only way i can try is to reduce the bias voltage to as less as possible, so i operated it at 70V for which the response is as below.

reasons are unknow for the expansion of 20ns pulse to 100ns even through the APD is having a BW of 70MHz,

so in order to operate the APD properly, i understood i have to bias with higher voltage to see proper response for low light, but at the same time i have to avoid saturation.

i feel limiting the current to the TIA will solve problem, kindly suggest some ways to bypass the excess current which is to the opamp.

Kindly throw some light on behaviour of APD in saturation also

Update: After few discussions over other forums online i understood that the ringing and over shoot are because of the unstability of LTC6269-10, even though i try to maintain the Cin/ Cf ratio of the decompensated opamp to 10 still the over shoot and ringing are seen why ? 

Kindly also suggest me few app notes to handle the APDs, i have seen few LT notes like AP92 but could not find matching circuits for mine, as mine is 300V bias

If this cannot be discussed on Analog forum, kindly forward this to the LT team

 

Thanks

Shyam Daram

Parents
  • i have found in my recent finding that the photo diode is sourcing too much current up to 50mA when light falls on , i have confirmed this from an resistor drop technique, using 100 ohm resistor.

    this is the main reason why i am facing these problems of too much overshoot.

    to over come this i have put a Schottky diode at the input of op-amp so that it will bypass the extra current, i simulated it on LT spice also, so i was able to avoid this over saturation to an extent, but i am facing new problems

    so in this process, i have damaged few Opamps also, this happened when i used it for long time(i really doubt the durability of LTC6269 also)

     

    my detector card has around 10 diodes for which i am using 5 ICs of LT6269(dual) , so even if one opamp is gone, as they share a common supply rail, i see the complete power rail shorted or the voltage appearing 1.1V instead of -2.5V.

    in one of my current card i am not able to identify which opamp is gone bad, how to identify a defective opamp??

    EDIT:in my boards i thought Op-amp is having short, but its actually the decoupling capacitors of 0.1uF, 25V 0603,ceramic going bad, they are going bad very frequently, kindly tell me what may be the reason for decoupling caps going bad

Reply
  • i have found in my recent finding that the photo diode is sourcing too much current up to 50mA when light falls on , i have confirmed this from an resistor drop technique, using 100 ohm resistor.

    this is the main reason why i am facing these problems of too much overshoot.

    to over come this i have put a Schottky diode at the input of op-amp so that it will bypass the extra current, i simulated it on LT spice also, so i was able to avoid this over saturation to an extent, but i am facing new problems

    so in this process, i have damaged few Opamps also, this happened when i used it for long time(i really doubt the durability of LTC6269 also)

     

    my detector card has around 10 diodes for which i am using 5 ICs of LT6269(dual) , so even if one opamp is gone, as they share a common supply rail, i see the complete power rail shorted or the voltage appearing 1.1V instead of -2.5V.

    in one of my current card i am not able to identify which opamp is gone bad, how to identify a defective opamp??

    EDIT:in my boards i thought Op-amp is having short, but its actually the decoupling capacitors of 0.1uF, 25V 0603,ceramic going bad, they are going bad very frequently, kindly tell me what may be the reason for decoupling caps going bad

Children
No Data