Dear Sir/Madam,
I Read the datasheet ADPD105-106-107.pdf and found that the default value of register 0x4B bit[15:9] is 0x13 (in the table at page 62), however, the "description" column of the table prints "Write 0x26" for bit[15:9]. IS IT CORRECT ? From the datasheet examples, the value of 0x4B always starts with "0x26" , for example, Register 0x4B=0x2612 in page 17. The example should be Register 0x4B=0x4C12 if "Write 0x26" for bit[15:9] is correct! So I am confused!