Post Go back to editing

Changing the Wavelengths in the MAX30101

Thread Summary

The user inquired about customizing an OFE module with 3 emitters and a PD system for wavelengths of 660, 805, and 940 nm, similar to the MAX30101 but with different wavelengths. The support engineer directed the user to Analog Devices' technical support pages for further assistance. No specific solution or product configuration was provided.
AI Generated Content
Category: Hardware
Product Number: MAX30101
I am looking to procure a custom OFE (optical front end) module that has 3 emitters + PD system correspdong to 660, 805 and 940 nm in a reflective sensor arrangement. An example of what I need is the MAX30101 package, except that the 3 emitters correspond to 525, 660, 880nm which means only 1 of the 3 wavelengths matches my interest. 
So, my question is, can AD repalce the OFE on the board with the wavelengths of my interest? Thank you for your assistance. 

Thread Notes

Parents Reply Children
No Data