Post Go back to editing

Temperature Estimate in a no flow enviroment

Thread Summary

The user is experiencing overheating issues with a DC-Motor driver when driving a Peltier module at 10V and 3.7A. The LT8722 was suggested as an alternative, with a thermal image showing the chip reaches 77°C at 15V input, 13.3V output, 3.83A current, and no airflow. Lowering the switching frequency can improve efficiency and reduce temperature rise.
AI Generated Content
Category: Hardware
Product Number: LT8722

Dear community members, 

im currently working on a project including a peltier module. Peltier specs are:
Imax: 7.5 A
Vmax (vdc): 17.5
AC Resistance (ohms): 1.66

On a lab bench powersupply i´ve reached my desired temperatures at 10 V and ~3.7 A

I was trying to use a DC-Motor driver to drive my TEC but in this application and max currents of up to 3.7 A my motor driver gets fairly hot (80° C) in ambient conditions. As it is planned to mount the circuit board in an enviroment with minimal to no airflow i searched for alternative components and found the LT8722 wich apparently is perfectly suitable for my application. 

I was wondering if anybody can give me a estimate how hot the chip gets with a constant current of 4 A in ambient conditions and if anybody has operated the device in an enviroment with barely any airflow available.

Getting the evaluation board is planned but i have to wait for my supervisor to come back from holiday. 

Thank you for the help in advance!

Thread Notes

Parents
  • Hello,

    The demo manual for the LT8722 demo board (DC3145A) shows a thermal image of the LT8722 on page 7 with these conditions:

    • VIN = 15V
    • VTEC = 13.3V
    • ITEC = 3.83A
    • L = COILCRAFT XGL4020-102MEC
    • FSW = 3MHz
    • No airflow
    • Tamb = 25 degrees C

    The LT8722 temperature reaches 77 degrees C and the efficiency is 95.1%. Using a lower switching frequency will provide higher efficiency and lower temperature rise. The demo board is a 4 layer design with dimensions of 3.0” x 3.0”. 

    Best regards,

    Mike

Reply
  • Hello,

    The demo manual for the LT8722 demo board (DC3145A) shows a thermal image of the LT8722 on page 7 with these conditions:

    • VIN = 15V
    • VTEC = 13.3V
    • ITEC = 3.83A
    • L = COILCRAFT XGL4020-102MEC
    • FSW = 3MHz
    • No airflow
    • Tamb = 25 degrees C

    The LT8722 temperature reaches 77 degrees C and the efficiency is 95.1%. Using a lower switching frequency will provide higher efficiency and lower temperature rise. The demo board is a 4 layer design with dimensions of 3.0” x 3.0”. 

    Best regards,

    Mike

Children
No Data