Post Go back to editing

Writing an image file to the microSD card on ADTF3175

Category: Hardware
Product Number: ADTF3175

Hello, I am trying to install an ToF camera EVAL-ADTF3175D-NXZ.

After installing the software (TOF_Evaluation_ADTF3175D-Rel6.0.1_EVAL.exe) on a Windows 10 Pro desktop PC, I connected the ToF camera to the PC with the attached USB Type-C cable.

But the ADIToFGUI program showed the following error messages:

--

I20250530 09:47:55.996219 17104 ADIToF.cpp:80] SDK version: 6.0.1 | branch: HEAD | commit: e748dbfd
I20250530 09:47:56.238046 17104 system_impl.cpp:88] SDK built with websockets version:3.1.0
I20250530 09:47:56.238046 17104 usb_sensor_enumerator.cpp:56] Looking for USB connected sensors
E20250530 09:47:56.242048 17104 usb_sensor_enumerator.cpp:79] Device Enumeration Error
I20250530 09:47:56.242048 17104 network_sensor_enumerator.cpp:66] Looking for sensors over network: 10.43.0.1
[2025/05/30 09:47:56:2440] NOTICE: Creating Vhost 'default' (serving disabled), 1 protocols, IPv6 off
W20250530 09:47:59.252058 17104 network_sensor_enumerator.cpp:71] Server Connect Failed

--

The error messages indicate that the program failed to find the ToF camera on USB ports.

The Troubleshooting Guide advises to "Ensure that the NXP SD card image is the one downloaded from the GUI installer."

So I am trying to do this, but the microSD card (16GB nominal), which has been kept inserted since shipping, shows only 147MB available as a USB drive on the PC, as listed below:

balenaEtcher does not allow me to write the image file to this microSD card, saying the available space is too small. 

The question is, may I destroy the original contents of this 16GB microSD card so that 16GB memory space is recovered?

Or, should I replace the microSD card itself?

Any advice will be greatly appreciated.

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.