Please kindly review and advise if they tested correctly or not.
- Connect USB-C to laptop (for additional connection options please check “Connectivity” section)
- The following leds must turn on before moving to next steps:
- Green led under USB-C connector
- Blinking led on NXP SOM
- Blue led on ADSD3500 interposer board
Problem :
As per the guide, we connected a Laptop and provided cable as C to C way, 3 LEDs are supposed to be turned on, but Blue LED is turned on for only two seconds and then off.
Even we ignored that Blue LED was turned off, and installed TOF_Evaluation_ADTF3175D-Rel5.0.0, then run ADIToFGUI from Bin, we encountered issue as shared in attachment.

AMD FA607P Series
Processor : AMD Ryzen
O/S :Windows 11 Home
Graphics : NVIDIA® GeForce RTX
Memory : 16GB DDR5-5200 SO-DIMM x 2, Max Capacity:32GB
I/O : 1x HDMI 2.1 FRL/1x RJ45 LAN port , 1x USB 3.2 Gen 2 Type-C support DisplayPort