Hi all,
I am wondering if the MAX30110 could drive two LEDs ON at the same time or have the pins connected in parallel to a single LED to increase the maximum available current to 400mA.
Cheers
MAX30110
Production
The MAX30110 is a complete optical pulse oximetry and heart rate detection integrated analog front-end. The MAX30110 has a high-resolution, optical readout...
Datasheet
MAX30110 on Analog.com
Hi all,
I am wondering if the MAX30110 could drive two LEDs ON at the same time or have the pins connected in parallel to a single LED to increase the maximum available current to 400mA.
Cheers