Post Go back to editing

ADPD10808 Sampling Frequency Jitter

Category: Hardware

Hello,

I noticed strong jittering when I output half the sampling frequency on one of the GPIO pins. I did a mean measurement with an oscilloscope (see picture). It shows an offset of up to 15 periods of the 32 kHz clock. All of the clock period offsets in this range are equally likely. What could be the cause of this?

Sampling frequency is 500 Hz. Only Slot A is enabled. GPIO0_ALT_CFG is set to 0x0F ("toggles on every sample, which provides a signal at half the sampling rate"). The 32 kHZ clock doesn't jitter when I output it on one of the GPIO pins.

Another problem: I tried setting one of the GPIO pins up according to the clock calibration section, but it is continuously high instead of sending pulses. The SLOTA interrupt doesn't need to be cleared, does it?
Can somebody help me see what I'm missing?

Best regards

PS: here is a video of the jitter

  • Hi,

    this was most likely a faulty ADPD1080 chip. I assembled another board a while ago (same PCB design) and the ADPD1080 chip on the second board doesn't showcase this jittering.

    Best regards.