I am using MAX40658 connected to driver SN65LVDT101
The Max40658 outputs need to be in two condition:
Out(+) – Out (-) > 100mV to get high level at SN65LVD101 or Out(+) – Out (-) < 100mV to get low level at SN65LVD101
can you advise me what is the configuration between them: pull up or down, serial capacitor or not
This is reference design using MAX3658 (the MAX40658 replace him)