Post Go back to editing

LT1328 powering & photodiode multiplexing

Category: Hardware
Product Number: LT1328

Hello,

I've 2 questions regrding LT1328 frontend.

1. Is it important to uso low-noise LDO for LT1328 powering ?

2.Will LT1328 performance be degraded if connecting 8 different photodiodes with 8 to 1 analog multiplexing... or a better way is to use one LT1328 per photodiode and then multiplex the digital outputs?

Thanks.

Sincerely,

Pavel.

Parents
  • Hi Pavel,

    The LT1328's high-pass filter rejects low frequency noise, however the pin 1 bias voltage is still susceptible to drift from variations to the supply voltage.  Please refer to second TOC on page 3 of the datasheet (Change in Voltage on Pin 1 vs Supply Voltage).  High frequency noise on the supply can lead to jitter on the TTL signals.  If a low noise LDO is not used, I would recommend making sure that the supply pin bypass filter caps can handle any high frequency noise on the supply line.

    Regarding multiplexing, I would recommend multiplexing the digital outputs rather than the analog inputs.

    Regards,

    Omar

  • Hi Omar,

    Thanks. So you think it would be wise to use low-noise LDOs ... like these ones (LDLN025 from ST and LT3045 from Analog Device) ? What about one LDO per one LT1328 ... or one LDO for multiple LT1328 will be also Ok ?

    multiplexing the digital outputs rather than the analog inputs

    Ok

    Sincerely,

    Pavel

  • Hi Pavel,

    Adding LDO will help to improve the noise performance. Whether using one or eight LDOs in your new design depends on your noise requirements for your system and the noise level from your supply. One LDO can supply eight infrared receivers but might not be optimal for noise performance if their locations are far away from each other.

    Best,

    Jane

Reply
  • Hi Pavel,

    Adding LDO will help to improve the noise performance. Whether using one or eight LDOs in your new design depends on your noise requirements for your system and the noise level from your supply. One LDO can supply eight infrared receivers but might not be optimal for noise performance if their locations are far away from each other.

    Best,

    Jane

Children