Post Go back to editing

ADPD4000/ADPD4001 FIFO and debug/run problem

I’m trying to read an impedance value with ADPD4000 connected to stm32L4, but I have two problems with the reading of the fifo buffer and the execution of the code.

  • About the fifo, I don’t why it does not fill or it fills up with no sense value. I attached a photo with the values that adc returns
  • To run the code without problems, I had to insert a delay step between every function. If I don't do this the code doesn't run or it runs badly. For example, if I do not insert the delay before adi_adpdssm_getFifoLvl(), the data available in the FIFO returns zero.

I followed the example code which is on the official repository. Here is my configuration..

//ADPD4000 Impedance measurement

                              {0x0009U, 0x0094U}, // 32MHz trim

                              {0x000BU, 0x02EAU}, // 1MHz trim

                              {0x000DU, 0x0D05U}, // Sampling rate, 0D05 for 300 Hz, 2710 for 100Hz, 09C4 for 400 Hz

                              {0x000FU, 0x0006U}, // 1MHz osc

                              //{0x000FU, 0x0001U}, // 32kHz osc

                              //enable timeslot A and set idle mode

                              {0x0010U, 0x0000U}, // Timeslot enable, 0100 Timeslots AB, 0000 Timeslots A

                              {0x0020U, 0x0002U}, // Float input 3&4, 5&6, 7&8 during sleep

                              {0x0021U, 0x0068U}, // IN7/IN8 configured as a differential pair (IN5-IN6 single ended). VC2 set to AVDD during sleep

                              {0x0022U, 0x0003U},// gpio0 out inverted,

                              {0x0023U, 0x0002}, // gpio0 interruput x (pin cgf0 configured as output)

                              {0x0014U, 0x8000U}, // fifo to int x (enable interrupt of x)          

                              {0x0006U, 0x0010U}, // FIFO interrupt generation threshold. Generate FIFO interrupt  during a FIFO write when the number of bytes in the FIFO exceeds this valuee. The                                                                            FIFO is 256 bytes

                              // Slots config

                              //////Timeslot A Impedance measurement on IN5 //////

                              ////// IN5 as single-ended input //////

                              {0x0100U, 0x0000U}, // CH2 disabled, input resistor 500 ohms

                              {0x0101U, 0x41DAU}, // Full AFE, TIA+BPF+INT+ADC

                              //{0x0101U, 0x40E6U}, //TIA, integrator, and ADC.

                              //enable IN6

                              {0x0102U, 0x0300U}, // IN6 to CH1, IN5 disabled. R11=100Kohm is used like a reference for impedence measurements.

                              {0x0103U, 0x5A45U}, // PRECON TO Vref, alternate VC2 on each subsequent Time Slot x vref to vdel (TIA_Vref+250mV)         

                              {0x0104U, 0xE209U}, // 100K GAIN both channels, vref=.9

                              {0x0105U, 0x0000U}, // LEDs off

                              {0x0106U, 0x0000U},// LEDs off

                              {0x0107U, 0x0110U}, // 16 PULSE 1 INT

                              {0x0108U, 0x0014U}, // 50 kHz pulse train, continuous TIA connection

                              {0x010AU, 0x0003U}, // INT Width

                              {0x010BU, 0x180FU}, // INT timing offset, 15.75us

                              //{0x010CU, 0x100FU}, // MOD pulse width and offset

                              {0x010CU, 0x0310U}, //Mod pulse width 3us, mod offset 16us

                              {0x010DU, 0x0099}, // CHOP

                              {0x010EU, 0x0000U}, // OFFSET

                              {0x010FU, 0x0000U}, // OFFSET

   {0x0110U, 0x0003U},// 3 BYTES SIG Number of bytes of signal data to be written to the FIFO for Time Slot x. Selectable between 0 bytes and four bytes.

#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <adi_adpd_driver.h>
#include "adi_adpd_ssm.h"
#include "adi_adpd_reg.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
SPI_HandleTypeDef hspi2;

UART_HandleTypeDef huart2;

/* USER CODE BEGIN PV */
tAdiAdpdDcfgInst dcfg_ADPD4000[28] ={

		//ADPD4000 Impedance measurement
		{0x0009U, 0x0094U}, // 32MHz trim
		{0x000BU, 0x02EAU}, // 1MHz trim
		{0x000DU, 0x0D05U}, // Sampling rate, 0D05 for 300 Hz, 2710 for 100Hz, 09C4 for 400 Hz
		{0x000FU, 0x0006U}, // 1MHz osc
		//{0x000FU, 0x0001U}, // 32kHz osc 
		///*il primo bit abilita l'oscillatore a 32, il secondo a 1M, il terzo selezione il  low frequency oscillator*/
		//abilito solo il timeslot A e setto il standby la modalità
		{0x0010U, 0x0000U}, // Timeslot enable, 0100 Timeslots AB, 0000 Timeslots A
		{0x0020U, 0x0002U}, // Float input 3&4, 5&6, 7&8 during sleep
		{0x0021U, 0x0068U}, // IN7/IN8 configured as a differential pair (IN5-IN6 single ended). VC2 set to AVDD during sleep
		//{0x0022U, 0x0403U}, // gpio0 out inverted, gpio3 output normal
		{0x0022U, 0x0003U},
		{0x0023U, 0x0002}, // gpio0 interruput x (pin cgf0 configured as output)
		{0x0014U, 0x8000U}, // fifo to int x (enable interrupt of x)	
		{0x0006U, 0x0010U}, //aggiunto io.FIFO interrupt generation threshold. Generate FIFO interrupt during a
												//FIFO write when the number of bytes in the FIFO exceeds this valuee. The FIFO is 256 bytes
		// Slots config
		//////Timeslot A Impedance measurement on IN5 //////
		////// IN5 as single-ended input //////
		{0x0100U, 0x0000U}, // CH2 disabled, input resistor 500 ohms
		{0x0101U, 0x41DAU}, // Full AFE, TIA+BPF+INT+ADC
		//{0x0101U, 0x40E6U}, //TIA, integrator, and ADC.
		//il registro 0x0102 si riferische ai canali attivi sulla board
		{0x0102U, 0x0300U}, // IN6 to CH1, IN5 disabled. R11=100Kohm is used like a reference for impedence measurements.
		//{0x0103U, 0x5A2CU}, // PRECON TO Vref, pulse VC2 vref to vdel (TIA_Vref+250mV)
		//{0x0103U, 0x5B05U},
		{0x0103U, 0x5A45U}, // PRECON TO Vref, alternate VC2 on each subsequent Time Slot x vref to vdel (TIA_Vref+250mV)	
		{0x0104U, 0xE209U}, // 100K GAIN both channels, vref=.9
		{0x0105U, 0x0000U}, // LEDs off
		{0x0106U, 0x0000U},// LEDs off
		{0x0107U, 0x0110U}, // 16 PULSE 1 INT

		{0x0108U, 0x0014U}, // 50 kHz pulse train, continuous TIA connection
		{0x010AU, 0x0003U}, // INT Width
		{0x010BU, 0x180FU}, // INT timing offset, 15.75us
		//{0x010CU, 0x100FU}, // MOD pulse width and offset
		{0x010CU, 0x0310U}, //Mod pulse width 3us, mod offset 16us
		{0x010DU, 0x0099}, // CHOP
		{0x010EU, 0x0000U}, // OFFSET
		{0x010FU, 0x0000U}, // OFFSET
		{0x0110U, 0x0003U},// 3 BYTES SIG Number of bytes of signal data to be written to the FIFO for Time Slot x. 
		//										Selectable between 0 bytes and four bytes.
		//{0x0110U, 0x0004U},// 4 BYTES SIG
		
		{0xFFFF, 0xFFFF}, //terminator
};
static tAdiAdpdSSmInst oAdiAppInst;
static uint8_t aFifoDataBuf[MAX_SAMPLES_IN_FIFO];
static uint16_t dev_id; uint16_t o_dri_res, res;
static uint8_t tx_buffer[1000];
static int command=0, kk=0;
static uint8_t gnAdpdDataReady = 0;
uint32_t gnAdpdTimeCurVal = 0;
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_SPI2_Init(void);
static void MX_USART2_UART_Init(void);
/* USER CODE BEGIN PFP */
static void tx_com( uint8_t *tx_buffer, uint16_t len );
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin);

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{
  /* USER CODE BEGIN 1 */

  /* USER CODE END 1 */

  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */
  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_SPI2_Init();
  MX_USART2_UART_Init();
  /* USER CODE BEGIN 2 */
	uint32_t adpd_ch1 = 0U;
  uint16_t loop = 0U;
  static uint32_t tick = 0U;
	/*Switch pin definition*/
	//HAL_GPIO_WritePin(GPIOG, GPIO_PIN_0, GPIO_PIN_RESET);
	HAL_GPIO_WritePin(GPIOF, GPIO_PIN_14, GPIO_PIN_SET);
	
	/*set CS pin */
	HAL_GPIO_WritePin(GPIOB, GPIO_PIN_13, GPIO_PIN_SET);
	
	uint16_t nRetVal;
	uint16_t nRegValue = 0U;
	
	uint16_t nAdpdFifoLevelSize;
	ADI_ADPD_COMM_MODE bus_mode;
	while(dev_id!=0x00C0)
		{
		o_dri_res=adi_adpddrv_OpenDriver();
		dev_id= adi_adpddrv_GetDevId();
		}
	sprintf((char *)tx_buffer, "Adi board recognized!\n\r");
	tx_com(tx_buffer, strlen((char const *)tx_buffer));
	bus_mode = adi_adpddrv_GetComMode();
	if (bus_mode != E_ADI_ADPD_SPI_BUS)
		{while(1);}
	HAL_Delay(100);
	/*load the config file. I had to add a verify control to be sure about the writing registers*/
	if (adi_adpdssm_loadDcfg(dcfg_ADPD4000, 0xFFU) != ADI_ADPD_SSM_SUCCESS)
		{
				while(1);
		}

	sprintf((char *)tx_buffer, "Adress configuration done!\n\r");
	tx_com(tx_buffer, strlen((char const *)tx_buffer));
	HAL_Delay(100);
	/*The function save configuration for each slot (12 slot) */
	adi_adpdssm_slotinit(&oAdiAppInst);
	HAL_Delay(10);
	 if (adi_adpdssm_setOperationMode(E_ADI_ADPD_MODE_SAMPLE) != ADI_ADPD_DRV_SUCCESS)
    {
        while(1);
    }
	nRetVal=adi_adpddrv_RegRead(ADPD4x_REG_INT_STATUS_FIFO, &nRegValue);
	sprintf((char *)tx_buffer, "Set Operation Mode done!\n\r");
	tx_com(tx_buffer, strlen((char const *)tx_buffer));
	HAL_Delay(10);
  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
		if (gnAdpdDataReady){
			gnAdpdDataReady=0;
			uint32_t nRetValue = 0U;
			// Not using ADPD400x auto clear int flag -> need to clear
			adi_adpddrv_RegWrite(ADPD4x_REG_INT_STATUS_DATA, 0x8000);
			/* Read the size of the data available in the FIFO */
			//nAdpdFifoLevelSize indicates 
			HAL_Delay(5);
			nRetValue = adi_adpdssm_getFifoLvl(&nAdpdFifoLevelSize);
			if (nRetValue != ADI_ADPD_DRV_SUCCESS)
				{
        while(1);
				};
			//nRetVal=adi_adpddrv_RegRead(ADPD4x_REG_FIFO_DATA, &nRegValue);
			/* Read the fifo data available in the FIFO */
			HAL_Delay(5);
			nRetValue = adi_adpddrv_ReadFifoData(nAdpdFifoLevelSize, &aFifoDataBuf[0]);
			if(nRetValue!=ADI_ADPD_DRV_SUCCESS)
			{
				while(1);
			};
			//nRetVal=adi_adpddrv_RegRead(ADPD4x_REG_FIFO_DATA, &nRegValue);
			tick=0;
			loop = 0U;
			adpd_ch1 = 0U;
			/* Read the data from the FIFO and print them */
			while (nAdpdFifoLevelSize != 0U) {
				/* Byte swapping is needed to print ADPD data in proper format */
				adpd_ch1 = ((aFifoDataBuf[loop] << 8) + (aFifoDataBuf[loop + 1]) +(aFifoDataBuf[loop + 2] << 24) + (aFifoDataBuf[loop + 3] << 16));	
				sprintf((char *)tx_buffer,
									"%u,%u\r\n", tick, adpd_ch1);
				tx_com(tx_buffer, strlen((char const *)tx_buffer));
				
				if(nAdpdFifoLevelSize>=oAdiAppInst.oAdpdSlotInst.nTotalSlotSz)
					{
						nAdpdFifoLevelSize -= oAdiAppInst.oAdpdSlotInst.nTotalSlotSz;
						loop += oAdiAppInst.oAdpdSlotInst.nTotalSlotSz;
						tick += 1;
					}
				else 
					nAdpdFifoLevelSize = 0U;
						
					
	}
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */
  }
		
}
  /* USER CODE END 3 */
}

/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
  RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};

  /** Configure the main internal regulator output voltage
  */
  if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
  {
    Error_Handler();
  }
  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
  RCC_OscInitStruct.HSIState = RCC_HSI_ON;
  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }
  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
  {
    Error_Handler();
  }
  PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART2;
  PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;
  if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
  {
    Error_Handler();
  }
}

/**
  * @brief SPI2 Initialization Function
  * @param None
  * @retval None
  */
static void MX_SPI2_Init(void)
{

  /* USER CODE BEGIN SPI2_Init 0 */

  /* USER CODE END SPI2_Init 0 */

  /* USER CODE BEGIN SPI2_Init 1 */

  /* USER CODE END SPI2_Init 1 */
  /* SPI2 parameter configuration*/
  hspi2.Instance = SPI2;
  hspi2.Init.Mode = SPI_MODE_MASTER;
  hspi2.Init.Direction = SPI_DIRECTION_2LINES;
  hspi2.Init.DataSize = SPI_DATASIZE_8BIT;
  hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
  hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;
  hspi2.Init.NSS = SPI_NSS_SOFT;
  hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
  hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
  hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
  hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
  hspi2.Init.CRCPolynomial = 7;
  hspi2.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
  hspi2.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
  if (HAL_SPI_Init(&hspi2) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN SPI2_Init 2 */

  /* USER CODE END SPI2_Init 2 */

}

/**
  * @brief USART2 Initialization Function
  * @param None
  * @retval None
  */
static void MX_USART2_UART_Init(void)
{

  /* USER CODE BEGIN USART2_Init 0 */

  /* USER CODE END USART2_Init 0 */

  /* USER CODE BEGIN USART2_Init 1 */

  /* USER CODE END USART2_Init 1 */
  huart2.Instance = USART2;
  huart2.Init.BaudRate = 115200;
  huart2.Init.WordLength = UART_WORDLENGTH_8B;
  huart2.Init.StopBits = UART_STOPBITS_1;
  huart2.Init.Parity = UART_PARITY_NONE;
  huart2.Init.Mode = UART_MODE_TX_RX;
  huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart2.Init.OverSampling = UART_OVERSAMPLING_16;
  huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
  huart2.Init.ClockPrescaler = UART_PRESCALER_DIV1;
  huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
  if (HAL_UART_Init(&huart2) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_SetTxFifoThreshold(&huart2, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_SetRxFifoThreshold(&huart2, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_DisableFifoMode(&huart2) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN USART2_Init 2 */

  /* USER CODE END USART2_Init 2 */

}

/**
  * @brief GPIO Initialization Function
  * @param None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};

  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOD_CLK_ENABLE();
  __HAL_RCC_GPIOG_CLK_ENABLE();
  HAL_PWREx_EnableVddIO2();
  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();
  __HAL_RCC_GPIOF_CLK_ENABLE();

  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(GPIOF, GPIO_PIN_14, GPIO_PIN_RESET);

  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(GPIOB, GPIO_PIN_13, GPIO_PIN_RESET);

  /*Configure GPIO pin : PG9 */
  GPIO_InitStruct.Pin = GPIO_PIN_9;
  GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);

  /*Configure GPIO pin : PF14 */
  GPIO_InitStruct.Pin = GPIO_PIN_14;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);

  /*Configure GPIO pin : PB13 */
  GPIO_InitStruct.Pin = GPIO_PIN_13;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_OD;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

  /* EXTI interrupt init*/
  HAL_NVIC_SetPriority(EXTI9_5_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(EXTI9_5_IRQn);

}

/* USER CODE BEGIN 4 */
static void tx_com(uint8_t *tx_buffer, uint16_t len)
{

  HAL_UART_Transmit(&huart2, tx_buffer, len, 5000);
}

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
	//gnAdpdTimeCurVal=HAL_GetTick();
	if(GPIO_Pin==GPIO_PIN_9)
	{
		gnAdpdDataReady=1;
		//adi_adpddrv_ISR(gnAdpdTimeCurVal);
	}
  /* Prevent unused argument(s) compilation warning */
  UNUSED(GPIO_Pin);

  /* NOTE: This function should not be modified, when the callback is needed,
           the HAL_GPIO_EXTI_Callback could be implemented in the user file
   */
}
/* USER CODE END 4 */

/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
  __disable_irq();
  while (1)
  {
  }
  /* USER CODE END Error_Handler_Debug */
}

Edit Notes

I attached also the main code
[edited by: Gloi at 8:23 AM (GMT -5) on 15 Feb 2021]
Parents
  • Hi Gloi,

    The data size is 3byte, which is based on configuration settings.

    So, you need to change your byte swapping order from 4 byte to 3 byte data size as below.

    /* Byte swapping is needed to print ADPD data in proper format */
    adpd_ch1 = ((aFifoDataBuf[loop] << 8) + (aFifoDataBuf[loop + 1]) + (aFifoDataBuf[loop + 2] << 16));

    Regards,
    Optical Support

  • Thank you for the reply, 

    I changed it, but is it normal that  " nAdpdFifoLevelSize " is not always a multiple of nTotalSlotSize, which is 3byte?

    I insert a check otherwise the while loop where the swapping is done becomes infinite

    Thanks,

    Gloi

  • Hi GlenBu,

    No, I don't have any other component between Vc2 and IN6. I tried to change timing of MOD pulse and integrator without success. I want only to calculate the capacitance to verify the entire system..

  • Hi Gloi,

    If you are interested in the capacitance measurement (capacitive load), you need to follow the guidance on capacitance measurement, page 35-36 of the ADPD4100 datasheet, to config your measurement and calculate the capacitance.

    Regards,

    Glen B.

  • Sorry GlenBu, 

    I'm using ADPD4000. However, I configured the registers in accord of page 32 of the ADPD4000 datasheet and I noticed that they are the same on ADPD4100. I'm interested in the impedance measurement,  but before starting I wanted to check that everything works. So, I connected a capacitance, I used this formula to calculate the current:

    current= ((0.92*((adpd_ch1-8196)/0.81)*(R_int/(2*Rf))/tpw)*pow(10, -9.0));
    //current= ((0.92*(adpd_ch1-8196)*(R_int/(2*Rf))/tpw)*pow(10, -9.0)); //without BFP

    and then 
    capacitance=(current)/(2*pi_greco*fsample*ex_volt);

    where fsample=50000 and ex_volt=0.25. Am I doing something wrong?

    Thanks,

    Gloi

  • Hi Gloi,

    The frequency in your capacitance measurement should be the frequency of the excitation pulse, not the sampling frequency.

    ADPD4000 can only measure amplitude rather than both amplitude and phase of the induced current. For accurate calculation, you would need both the amplitude and the phase. 

    Regards,

    Glen B.

  • fsample is the frequency of the pulse train, I'm sorry the name can be confusing. It is setted writing 0x0108U register to  0x0014U.

    Regards,

    Gloi

  • Hi GlenBu, 

    I set the timing registers trying to keep the datasheet rules. Now, when I don't connect any capacitors to the input, the ADC returns a value equal to 8210. Similar to the offset, so it seems ok. However,  I'm not still able to measure different value of capacitor. It seems that ADC saturates for every capacitor that i inserted.

    Regards,

    Gloi

    EDIT: I tried also to change TIA gain, but the ADC returns always similar values for different capacitors.

    I noticed, even though i write the signal data on four bytes, only two bytes are written and updated always. The first two are always zero

  • Hi Gloi,

    You might want to play with the integrator time offset so that the integration is done on the pulses. You might also want to test with a resistor instead of a capacitor to simplify the timing.

    Regards,

    Glen B

  • Thanks GlenBu, 

    I tried to change the integrator time offset in different ways without success and considering always the figure 38-39 on the datasheet. But I do not understand why the first two byte of the signal. I also read the registers SIGNAL1_L_A (0x0030) and SIGNAL1_H_A (0x0031)and the last one is always zero. 

    Do you have any other idea about that?

    BR, 

    Gloi

  • Hi Gloi,

    Honestly I have no idea of your problem. Please make sure that your software reads FIFO correctly. You may want to test your setup with some simple tasks that you know the answer. 

    Good luck!

    Glen B.

  • Hi GlenBu, 

    Now I'm able to read the correct value of the impedance, but I noticed another problem about the FIFO. 

    I configured the register 0x000D to obtain a sampling frequency of 300Hz, but if I register the signal for one minute I obtain a sampling frequency about 100Hz.

    I saw the register 0x0000 and discovered that I have an overflow of the FIFO. I tried to introduce Decimate_Factor, but if I introduce it, the code does not work, like also if I reduce to 100Hz the sampling rate (I don't understand why). 

    Here my new config.

    tAdiAdpdDcfgInst dcfg_ADPD4000[32] ={
    //ADPD4000 Impedance measurement
    {0x0009U, 0x0094U}, // 32MHz trim high frequency oscillator controls the AFE operations
    {0x000BU, 0x02EAU}, // 1MHz trim low frequency oscillator sets the time base used to control the sample timing, wake-up states, and overall operation
    {0x000CU, 0x8012U}, // Enable time stamp capture, 32kHz oscillator trim at default frequency
    {0x000DU, 0x0d05U}, // Sampling rate, 0D05 for 300 Hz, 2710 for 100Hz, 09C4 for 400 Hz,1388 for 200Hz
    {0x000FU, 0x0006U}, // 1MHz osc
    {0x0010U, 0x0000U}, // Timeslot enable, 0100 Timeslots AB, 0000 Timeslots A
    {0x0020U, 0x0002U}, // Float input 3&4, 5&6, 7&8 during sleep
    {0x0021U, 0x0068U}, // IN7/IN8 configured as a differential pair (IN5-IN6 single ended). VC2 set to AVDD during sleep

    {0x0022U, 0x0443U}, // gpio0 out inverted, gpio2 output normal
    {0x0023U, 0x0002U}, // gpio0 interruput x (pin cgf0 configured as output)
    {0x0024U, 0x0002U}, //gpio2 for time stamp,
    {0x0026U, 0x0060U}, //gpio2 for time stamp,
    {0x0014U, 0x8000U}, // fifo to int x (enable interrupt of x)
    {0x0006U, 0x0080U}, /
    // Slots config
    //////Timeslot A Impedance measurement on IN6 //////
    ////// IN6 as single-ended input //////

    {0x0100U, 0x0000U},
    {0x0101U, 0x41DAU}, // Full AFE, TIA+BPF+INT+ADC

    {0x0102U, 0x0300U}, // IN6 to CH1, IN5 disabled. R11=100Kohm is used like a reference for impedence measurements.

    {0x0103U, 0x5A45U}, // PRECON TO Vref, alternate VC2 on each subsequent Time Slot x vref to vdel (TIA_Vref+250mV)

    {0x0104U, 0xE209U},//
    {0x0105U, 0x0000U}, // LEDs off
    {0x0106U, 0x0000U},// LEDs off


    {0x0107U, 0x0107U}, // 07/0B/1F/23/33 finali

    {0x0108U, 0x0014U},

    {0x0112U, 0x0000U},


    {0x010CU, 0x0306U},// MOD pulse width and offset


    {0x010AU, 0x0005U}, //INT Width

    {0x010BU, 0x0304U}, //

    {0x010DU, 0x0099U}, // CHOP
    {0x010EU, 0x0000U}, // OFFSET
    {0x010FU, 0x0000U}, // OFFSET

    // Selectable between 0 bytes and four bytes.
    {0x0110U, 0x0004U},// 4 BYTES SIG
    //{0x0110U, 0x0003U},// 3 BYTES SIG
    {0xFFFF, 0xFFFF}, //terminator


    };

Reply
  • Hi GlenBu, 

    Now I'm able to read the correct value of the impedance, but I noticed another problem about the FIFO. 

    I configured the register 0x000D to obtain a sampling frequency of 300Hz, but if I register the signal for one minute I obtain a sampling frequency about 100Hz.

    I saw the register 0x0000 and discovered that I have an overflow of the FIFO. I tried to introduce Decimate_Factor, but if I introduce it, the code does not work, like also if I reduce to 100Hz the sampling rate (I don't understand why). 

    Here my new config.

    tAdiAdpdDcfgInst dcfg_ADPD4000[32] ={
    //ADPD4000 Impedance measurement
    {0x0009U, 0x0094U}, // 32MHz trim high frequency oscillator controls the AFE operations
    {0x000BU, 0x02EAU}, // 1MHz trim low frequency oscillator sets the time base used to control the sample timing, wake-up states, and overall operation
    {0x000CU, 0x8012U}, // Enable time stamp capture, 32kHz oscillator trim at default frequency
    {0x000DU, 0x0d05U}, // Sampling rate, 0D05 for 300 Hz, 2710 for 100Hz, 09C4 for 400 Hz,1388 for 200Hz
    {0x000FU, 0x0006U}, // 1MHz osc
    {0x0010U, 0x0000U}, // Timeslot enable, 0100 Timeslots AB, 0000 Timeslots A
    {0x0020U, 0x0002U}, // Float input 3&4, 5&6, 7&8 during sleep
    {0x0021U, 0x0068U}, // IN7/IN8 configured as a differential pair (IN5-IN6 single ended). VC2 set to AVDD during sleep

    {0x0022U, 0x0443U}, // gpio0 out inverted, gpio2 output normal
    {0x0023U, 0x0002U}, // gpio0 interruput x (pin cgf0 configured as output)
    {0x0024U, 0x0002U}, //gpio2 for time stamp,
    {0x0026U, 0x0060U}, //gpio2 for time stamp,
    {0x0014U, 0x8000U}, // fifo to int x (enable interrupt of x)
    {0x0006U, 0x0080U}, /
    // Slots config
    //////Timeslot A Impedance measurement on IN6 //////
    ////// IN6 as single-ended input //////

    {0x0100U, 0x0000U},
    {0x0101U, 0x41DAU}, // Full AFE, TIA+BPF+INT+ADC

    {0x0102U, 0x0300U}, // IN6 to CH1, IN5 disabled. R11=100Kohm is used like a reference for impedence measurements.

    {0x0103U, 0x5A45U}, // PRECON TO Vref, alternate VC2 on each subsequent Time Slot x vref to vdel (TIA_Vref+250mV)

    {0x0104U, 0xE209U},//
    {0x0105U, 0x0000U}, // LEDs off
    {0x0106U, 0x0000U},// LEDs off


    {0x0107U, 0x0107U}, // 07/0B/1F/23/33 finali

    {0x0108U, 0x0014U},

    {0x0112U, 0x0000U},


    {0x010CU, 0x0306U},// MOD pulse width and offset


    {0x010AU, 0x0005U}, //INT Width

    {0x010BU, 0x0304U}, //

    {0x010DU, 0x0099U}, // CHOP
    {0x010EU, 0x0000U}, // OFFSET
    {0x010FU, 0x0000U}, // OFFSET

    // Selectable between 0 bytes and four bytes.
    {0x0110U, 0x0004U},// 4 BYTES SIG
    //{0x0110U, 0x0003U},// 3 BYTES SIG
    {0xFFFF, 0xFFFF}, //terminator


    };

Children
  • Hi Gloi,

    You might want to lower your FIFO threshold setting in register 0x0006. In addition, I would suggest that you remove the timestamp capture related register setting 0x000C, 0x0024 and 0x0026 before you get the FIFO read work properly.

    Regards,

    Glen B.

  • Hi GlenBu,

    Thanks for the answer, but the problem remains. I tried also to read data from the FIFO in Polling mode, but also in this case I have an overflow. 

    I tried also to read directly 0x0031 and 0x0030 registers, I record the signal in polling mode, but I obtain the same frequency of 100Hz, also if I setted the register 0x000DU to  0x09c4U (400 Hz).

    Regards,

    Gloi

  • Hi Gloi,

    What did you observe when you decreased the FIFO threshold? Low FIFO threshold can prevent the FIFO from overflow. If you haven't done so, please test it. 

    Since you run only one timeslot, you should be able to achieve sampling rate up to kHz level. 

    Are you using SPI (ADPD4000) or I2C (ADPD4001)? Also, please check on you micro side if there is anything abnormal. Are you using SPI or I2C?

    As suggested previously, you may want to remove the timestamp capture related settings.

    Regards,

    Glen

  • Hi GlenBu, 

    The problem was the USART. It takes too long time to write data and meanwhile the fifo saturated

    BR, 

    Gloi

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.