KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
ADPD103
Not Recommended for New Designs
The ADPD103 is a highly efficient photometric front end with an integrated 14-bit analog-to-digital converter (ADC) and a 20-bit burst accumulator that...
Datasheet
ADPD103 on Analog.com
Dear Sir,
Does ADPD103 can drive a LED ( 5V~7V@20mA ) by the following Schematic? And the VCC is 8V.
Hi Kevin,
There is somethings puzzle me about the numbers of LED pulses. For example, assuming that I configure the ADPD103 into the Digital Integration mode, set the number of LED pulse to one pulse, and get 4000 form the ADC register. While, when I set to 10 LED pulses, the value of ADC is 45000, and 20 pluses is 90000, 30 pluses is 135000.
I cannot understand that. In my eyes, when the pulse is 10, the value may be about 10*4000= 40000, and pluse is 20, it will be about 20*4000 = 80000.
In Digital Integration mode, the registers of LED and AFE is setting as following.
0x30 0A19,
0x39 2184,
Hi Kevin,
There is somethings puzzle me about the numbers of LED pulses. For example, assuming that I configure the ADPD103 into the Digital Integration mode, set the number of LED pulse to one pulse, and get 4000 form the ADC register. While, when I set to 10 LED pulses, the value of ADC is 45000, and 20 pluses is 90000, 30 pluses is 135000.
I cannot understand that. In my eyes, when the pulse is 10, the value may be about 10*4000= 40000, and pluse is 20, it will be about 20*4000 = 80000.
In Digital Integration mode, the registers of LED and AFE is setting as following.
0x30 0A19,
0x39 2184,