KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
ADPD103
Not Recommended for New Designs
The ADPD103 is a highly efficient photometric front end with an integrated 14-bit analog-to-digital converter (ADC) and a 20-bit burst accumulator that...
Datasheet
ADPD103 on Analog.com
Dear Sir,
Does ADPD103 can drive a LED ( 5V~7V@20mA ) by the following Schematic? And the VCC is 8V.
Hi Kevin,
I am sure that the PD is connected correctly. And I will capture the voltage of the anode and cathode with an oscilloscope.
However, another question is about the input voltage of the ADC. I mean when I set ADPD103 to TIA mode, the TIA output is connected to the input of ADC. And what is the range of the TIA output voltage or ADC input voltage?
Thanks and Regards,
Danvy
Hi Kevin,
I am sure that the PD is connected correctly. And I will capture the voltage of the anode and cathode with an oscilloscope.
However, another question is about the input voltage of the ADC. I mean when I set ADPD103 to TIA mode, the TIA output is connected to the input of ADC. And what is the range of the TIA output voltage or ADC input voltage?
Thanks and Regards,
Danvy