KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
ADPD103
Not Recommended for New Designs
The ADPD103 is a highly efficient photometric front end with an integrated 14-bit analog-to-digital converter (ADC) and a 20-bit burst accumulator that...
Datasheet
ADPD103 on Analog.com
Dear Sir,
Does ADPD103 can drive a LED ( 5V~7V@20mA ) by the following Schematic? And the VCC is 8V.
Hi Danvy,
The PDC voltage only affects the voltage at the cathode of the photodiode, which should be connected to the PDC pin. The anode of the photodiode is connected to one of the PD inputs and the bias at that node is set by register 0x42 and 0x44 as mentioned in a previous response. Changing the cathode voltage of the PDC pin from 1.3V to 1.8V will only change the reverse bias across the photodiode. Assuming that you have everything connected correctlyI can't think of a reason that you would see the output of the device rail one way or the other based simply on the change in reverse bias of the PD. Please do the following:
1. Make sure that you have the PD corrected correctly
2. measure the voltages at the anode and cathode of the PD. You'll need to do this with an oscilloscope to see what the voltages are during the sampling period since they will both go to VDD during the sleep time.
3. Verify that you have the correct timing for digital integration mode based on the description in the datasheet.
Regards,
Kevin
Hi Danvy,
The PDC voltage only affects the voltage at the cathode of the photodiode, which should be connected to the PDC pin. The anode of the photodiode is connected to one of the PD inputs and the bias at that node is set by register 0x42 and 0x44 as mentioned in a previous response. Changing the cathode voltage of the PDC pin from 1.3V to 1.8V will only change the reverse bias across the photodiode. Assuming that you have everything connected correctlyI can't think of a reason that you would see the output of the device rail one way or the other based simply on the change in reverse bias of the PD. Please do the following:
1. Make sure that you have the PD corrected correctly
2. measure the voltages at the anode and cathode of the PD. You'll need to do this with an oscilloscope to see what the voltages are during the sampling period since they will both go to VDD during the sleep time.
3. Verify that you have the correct timing for digital integration mode based on the description in the datasheet.
Regards,
Kevin