Post Go back to editing

ADPD103 Drives a LED ( 5V~7V@20mA )

Dear Sir,

         Does ADPD103 can drive a LED ( 5V~7V@20mA ) by  the following Schematic? And the VCC is 8V. 

Parents
  • For some reason I assumed that we were talking about the ADPD105 since it's the latest device in the family. If this is a new design, then you should be looking at the ADPD105 (or ADPD107 if you wanted SPI). The ADPD105 is backwards compatible. There is more detail included in the datasheet with respect to some of the registers. For example, register 0x42/44, you will see the detail on bits [5:4] for the TIA_VBIAS

    0844.4857d40b946e0370b2b265b666528d1f.png

    Sorry for the confusion.

    Regards,

    Kevin

Reply
  • For some reason I assumed that we were talking about the ADPD105 since it's the latest device in the family. If this is a new design, then you should be looking at the ADPD105 (or ADPD107 if you wanted SPI). The ADPD105 is backwards compatible. There is more detail included in the datasheet with respect to some of the registers. For example, register 0x42/44, you will see the detail on bits [5:4] for the TIA_VBIAS

    0844.4857d40b946e0370b2b265b666528d1f.png

    Sorry for the confusion.

    Regards,

    Kevin

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.