Post Go back to editing

ADPD103

Thread Summary

The user encountered issues with the EVAL-ADPD103Z-GEN evaluation board not being recognized by the GUI after a firmware upgrade. The final answer suggests that the issue was resolved offline or through a multi-part answer. Accompanying answers recommend checking the COM port in Device Manager, ensuring FTDI drivers are installed, and verifying the connection with a terminal program. Another user reported a similar issue with the EVAL-ADPD105Z, but no specific solution was provided in the thread.
AI Generated Content

I am using an analog devices Eval board ADPD103Z-GEN, but the GUI is not recognizing the port for some reason. I was trying to do a firmware upgrade and after the download, when prompted for reset, it exit immediately! I suspect this is the cause of configuration fail! Is there any way I can configure the Eval board again?

Thread Notes

  • Does the COM port show up in device manager?

    These evaluation boards use a FTDI chip to provided a virtual com port through USB.  The FTDI drivers are typically automatically discoverable by windows and other OS systems.  In the even this does not occur you can go directly to the FTDI site and attempt do download the driver.

    Here is the link to the FTDI site to download VCP drivers.

    Virtual COM Port Drivers

    When successful the board should show up in the "com" port list of "Device Manager" if you are using a windows system.  It will show up as "USB Serial Port (COMXX)" where "XX" is the assigned com port number.

  • Hello,

    Could you please upload the documents relevant to the schematics of the

    eval board?

    On Fri, May 27, 2016 at 9:28 PM, Neal.Kurfiss <

  • The schematics are in the process of being placed on the web-site.  hopefully they will be in place by tomorrow.

  • The schematics and layout files are now up in the documents section of the EVAL-ADPD103Z-GEN evaluation board page.

  • Hi,

    I am still struggling with the connection of EVAL-ADPD103Z-GEN and any of my computers. I got the "USB Serial Port (COM5)" and I can connect with an terminal program but if i start the GUI and press the connect (Auto Connect and Select Port), I always get some error messages. "Target not found" "Select Proper COM Port". Do you have any idea how to get the EVAL-ADPD103Z-GEN running?

    I cannot do any Firmwareupdates because i need to connect first.

  • Dear Elglatze

    I faced the same issue on my EVAL-ADPD105Z. Did you get the idea to solve this?

    B/R

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.