Dear sirs,
The peak LED current of ADPD1080 is 250 mA. How you would suggest to use the device in a compact design powered by a coin battery e.g. CR3032? Such batteries are probably not able to sink such current.
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
ADPD1080
Recommended for New Designs
The ADPD1080/ADPD1081 are highly efficient, photometric front ends, each with an integrated 14-bit analog-to-digital converter (ADC) and a 20-bit burst...
Datasheet
ADPD1080 on Analog.com
Dear sirs,
The peak LED current of ADPD1080 is 250 mA. How you would suggest to use the device in a compact design powered by a coin battery e.g. CR3032? Such batteries are probably not able to sink such current.
Assuming the LED duty cycle is low , i.e. the LED on time is very much smaller that the LED off time , then a similar technique to that used in Infra Red Remote control units for a TV can be used .
The technique involves connecting a low ESR capacitor of usually somewhere between 4.7uF and 10 uF between the LED supply and the LED ground return . It should be easy to establish the actual value required using an oscilloscope. What you are looking for is minimal pulse "droop".
An example of this is shown in Fig 36 on page #31 of the datasheet .
One capacitor can be used for all three LED's or an individual capacitor for each LED , sizing the actual value ('s) appropriately of course.
It works like this :- While the LED's are off the capacitor, is charging up to the LED supply voltage . When the LED is turned on the capacitor is providing the peak current required and not the coin cell. When the LED is off the cycle repeats.
Assuming the LED duty cycle is low , i.e. the LED on time is very much smaller that the LED off time , then a similar technique to that used in Infra Red Remote control units for a TV can be used .
The technique involves connecting a low ESR capacitor of usually somewhere between 4.7uF and 10 uF between the LED supply and the LED ground return . It should be easy to establish the actual value required using an oscilloscope. What you are looking for is minimal pulse "droop".
An example of this is shown in Fig 36 on page #31 of the datasheet .
One capacitor can be used for all three LED's or an individual capacitor for each LED , sizing the actual value ('s) appropriately of course.
It works like this :- While the LED's are off the capacitor, is charging up to the LED supply voltage . When the LED is turned on the capacitor is providing the peak current required and not the coin cell. When the LED is off the cycle repeats.