Article What is the total input power requirement for the MAX86141?

The 3.1V - 5V requirement for VLED does need to be considered when looking at the power requirements for the MAX86140/1, alongside the 1.8V Vdd requirement. 

The VLED voltage is used to power the external LEDs which will be connected to the device. This voltage is generated external to the MAX86140/1.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.